Recent blog posts
  • Behind the Wheel
    • Dec 12, 2018

    Understanding how driver monitoring systems can help with collision avoidance, part 2

    Driver monitoring systems (DMS) are enhancing real-time feedback to a vehicle’s steering and control systems, as discussed in our recent post, “How driver monitoring systems can help with collision avoidance.” However, there ar...
  • Think. Innovate
    • Dec 11, 2018

    A voice for change: Erika Beskar’s boldness drives technology and others’ success

    When Erika Beskar accepts a challenge, she’s all in. “She’s extremely passionate about what she does,” said Lakshmi Holehonnur, an engineer at our company whom Erika mentored as part of a program to advance women in technical...
  • Industrial Strength
    • Dec 11, 2018

    Enhancing DAQ performance for grid protection, control and monitoring equipment, using DC/DC power modules

    (Note: Akshay Mehta co-authored this blog post.) In my previous blog posts on improving data acquisition (DAQ) performance for grid protection, control and monitoring equipment, I discussed the need for interfacing multiple analog-to-digital converters (ADCs) and showed how you can improve DAQ performance and measurement accuracy by using the programmable...
  • オートモーティブ
    • Dec 11, 2018

    EMI性能の向上に有効なマルチチャネル降圧コンバータ・レイアウトはどれか

    設計者は、多数の電源レールをサポートする車載機器システムに複数のDC/DC降圧コンバータをよく使用します。しかし、そのようなタイプの降圧コンバータを選ぶときには考慮すべき点があります。例えば、AMラジオ帯域との干渉を避けるために、車載インフォテインメント/ヘッド・ユニット用に(2MHz以上で動作する)高スイッチング周波数のDC/DCコンバータを選ばなければなりません。また、比較的小型のインダクタを選んで、ソリューション・サイズも小さくする必要があります。それに加えて、高スイッチング周波数DC/D...
  • オートモーティブ
    • Dec 11, 2018

    DC/DCコンバータのパッケージおよびピン配置設計により車載EMI性能を強化する方法

    DC/DC降圧コンバータや昇圧コンバータの電磁干渉(EMI)の削減を図る上で、プリント基板(PCB)のレイアウトが鍵となることはよく知られていますが、非常に低いEMIが求められる 車載用ゲートウェイ・モジュール や レーダ・センシング・システム などの車載用アプリケーションでは特に重要です。 図1の回路図は、同期整流降圧コンバータ回路の2つの重要なループを示しています。レイアウトの電源ループ領域の大きさは寄生インダクタンスとそれに関連する磁界の伝播に比例するため、最小限に抑えることが必須となります。 図...
  • アナログ
    • Dec 11, 2018

    超音波テクノロジによってホーム・オートメーションの利便性と性能を向上させる方法

    照明、ファン、サーモスタット、テレビ、音楽機器、ガレージ・ドア、玄関のチャイムなどの制御の自動化についての関心が高まっていることで、商用ビルディング・オートメーション・テクノロジを住宅に導入する傾向がますます強まっています。例えば、Amazon Alexa、Google Home、Apple HomePodおよびHomeKit、Winkのほか、多数のセントラル・ハブ製品が、住居内の各種電気/電子デバイスを制御および監視しています。(図1) 図1:動作検出や存在検出を備えた一般的なホーム・オートメ...
  • Industrial Strength
    • Dec 10, 2018

    Using smart relay drivers for smart meters, part 2

    In part 1 of this series, my colleague Shreenidhi Patil discussed the two most popular types of latching relays used in smart meters: a single-coil relay and a dual-coil relay. In this installment, I will explore TI’s offerings for relay-driving applications, including typical schematics and waveforms. Also, for an application-level understanding...
  • Analog Wire
    • Dec 7, 2018

    How to achieve rapid temperature sensor design with RTD-level accuracy and no calibration

    For the highest accuracy temperature measurement, system designers have traditionally had only one option: platinum resistive temperature detectors (RTDs) such as the PT100 or PT1000. Highly linear and interchangeable, RTDs are available in a wide range of accuracy classes as defined by International Electrotechnical Commission (IEC) and Deutsches Institut...
  • アナログ
    • Dec 7, 2018

    洗練されたロボットのための超音波式検出の利用

    現在、人間が行っている作業の多くをロボットが行うようになる日は、遠い先のことではありません。私たちはすでに、ロボット掃除機に部屋の掃除をさせたり、ロボット芝刈機に庭の草刈りをさせたりしています。工場では、歯ブラシから自動車まで、私たちが使用する多くの製品をロボットが製造しています。中国や日本ではロボットが料理を運び、ドローンによる肥料の散布や商品の配送も行われています。ですから、ロボットが家を建てたり、道路を敷いたり、クルマを運転したりする日も近いことでしょう。しかし、そのような未来を現実にするための重要な要件の1つは、ロボットが人間と同じような感覚を持つことです。 ロボット機器の最大の課題の1つは、壁や家具、設備、人間、他のロボットなどに衝突することのない移動経路をどのように見つけるかです...
  • Behind the Wheel
    • Dec 6, 2018

    Designing daytime running lights, part 2: responding to an LED fault

    This is the second installment in a two-part series on designing bright daytime running lights (DRLs) without the need for two LED drivers, a method provided in the Automotive Daytime Running Light Dual String LED Driver Reference Design with Current...
  • その他産業用
    • Dec 5, 2018

    振動解析によるモーター故障予知、第2部

    モーターやポンプは、工場や建物の重要なインフラストラクチャ・コンポーネントであり、その役割を果たすには適切な動作状態が保たれる必要があります。モーターやポンプの役割は、オートメーション・ライン上の物を動かしたり、暖房、換気、空調(HVAC)システム用に冷却液や冷却空気を流したりなどさまざまです。 どんなときであっても、性能低下はメンテナンス費用がかさむことになりかねません。あるいは故障により製造能力が停止状態になるかもしれません。十分な性能を維持するには、これらの機械の潜在的故障の徴候を監視する...
  • その他産業用
    • Dec 5, 2018

    状況監視による故障予知、第1部

    工場での製造活動には多数のモーターやポンプが不可欠です。その機能が故障すると、ラインが完全にストップしてしまうことになりかねません。これを防ぐために通常は幅広い予防保守計画を準備しておき、定期的に実施する必要があります。このような計画は寿命統計に基づくもので、機器の実際の状況には基づいていません。 機器の状況がわかれば、メンテナンス費用を削減でき、予期しない故障の危険性も減らすことができます。機器の状態を認識して修理や交換の予定を立てることを、予防保守と言います。 故障に至るプロセス最終的に機能...
  • Analog Wire
    • Dec 5, 2018

    The ADC12DJ3200 wins product of the year at World Electronics Achievement Awards

    The ultra-high-speed ADC12DJ3200 analog-to-digital converter (ADC) has won product of the year in the Amplifier/Data Conversion category of the inaugural World Electronics Achievement Awards (WEAAs) . Editors and readers voted it a winner in a worldw...
  • Power House
    • Dec 5, 2018

    Improving data-center efficiency with eFuses

    According to Forbes, global data centers used approximately 416TW (4.16 × 1014W) of electricity in 2017, with U.S. data centers contributing about 90 billion kilowatt hours to that number. With artificial intelligence making strides and 5G arou...
  • Behind the Wheel
    • Dec 4, 2018

    Designing daytime running lights, part 1: adding one-fail-all-fail LED fault detection

    Daytime running lights (DRLs) are becoming more popular in vehicles and are even a requirement in some countries. As I’m sure you can guess, DRLs are on during the day, which requires them to be very bright. As a designer, you typically have two choices to achieve the desired DRL LED brightness: Increase the number of LEDs in your string...