I have always proposed that the market for 8-bit processors would not fade away – in fact there are still a number of market niches that rely on 4-bit processors (such as clock movements and razor blades that sport a vibrating handle for men when shaving their faces). The smaller processor architectures can support the lowest cost price points and the lowest energy consumption years before the larger 32-bit architectures can begin to offer anything close to parity with the smaller processors. In other words, I believe there are very small application niches that even 8-bit processors are currently too expensive or energy hungry to support just yet.

Many marketing reports have identified that the available software development tool chains play a significant role in whether a given processor architecture is chosen for a design. It seems that the vast majority of resources spent evolving software development tools are focused on the 32-bit architectures. Is this difference in how software development tools for 8- and 32-bit processors are evolving affecting your choice of processor architectures?

I believe the answer is not as straight forward as some processor and development tool providers would want to make it out to be. First, 32-bit processors are generally much more complex to configure than 8-bit processors, so the development environments, which often include drivers and configuration wizards, are nearly a necessity for 32-bit processors and almost a non-issue for 8-bit processors. Second, the type of software that 8-bit processors are used for are generally smaller and contend with less system-level complexity. Additionally, as embedded processors continue to find their way into smaller tasks, the complexity of the software may need to be simpler than current 8-bit software to meet the energy requirements of the smallest subsystems.

Do you feel there is a significant maturity difference between software development tools targeting 8- and 32-bit architectures? Do you think there is/will be a widening gap in the capabilities of software development tools targeting different size processors? Are software development tools affecting your choice of using an 8-bit versus a 32-bit processor or are other considerations, such as the need for additional performance headroom for future proofing, driving your decisions?

Visit Embedded Insights to see the full conversation occurring across multiple communities about this and other questions of the week.

Anonymous