Why should you care about the noise immunity of MLVDS drivers and receivers?


Noise immunity is the ability of a device or system to suppress external noise, and to function – without deteriorating in performance – in the presence of noise. Multipoint low-voltage differential (MLVDS) devices are used widely in wired communication, optical communication and backplane applications, which are often located in harsh and noisy environments. To increase the robustness of MLVDS devices requires a high level of noise immunity performance.

How is noise immunity measured?

Noise immunity is measured by connecting an MLVDS driver to an MLVDS receiver in point-to-point mode and measuring the noise power in decibel-milliwatts over a frequency range. Figure 1 shows a noise immunity measurement test setup with TI’s SN65MLVD206B and SN65MLVD206B transceivers connected in a point-to-point topology. Note the 100Ω termination resistor placed between the LVDS bus. A coupling network with a 120Ω resistor and 4.7nF capacitor is used for common-mode (CM) noise injection. A clock signal input to the driver measures the impact of injected CM noise. After injecting CM noise into the LVDS bus through the resistor-capacitor (RC) coupling network, you can measure the subsequent output jitter. The measured output jitter over frequency translates to the noise immunity in decibel-milliwatts, as shown in Figure 2.

Figure 1: Noise immunity test setup

Figure 2: Noise immunity level over frequency

A noise immunity test is based on a mask test. As Figure 3 shows, the yellow waveform is the output signal of an MLVDS receiver without noise injected. The white mask indicates the 0.2 unit interval (UI) jitter limit. For a given noise frequency, the mask test starts with the maximum injected noise power, which you set manually. If the output jitter violates the mask, the injected noise power decreases in large steps until the output jitter no longer violates the mask limits. The injected noise power then increases in small steps until a violation occurs. The noise immunity level for this frequency is the maximum injected noise power that does not violate the output jitter mask.

Figure 3: Noise immunity mask test without noise injection

Why is noise immunity important?

Figure 4 shows several MLVDS receiver output signals impacted by injected noise. As you can see, the higher the noise power, the worse the signal.

Figure 4: Noise immunity mask test with noise injection (mask violation)

If the injected noise power exceeds the noise immunity level for a specified noise frequency, the excessive jitter will violate the mask. But if the injected noise power is lower than the noise immunity level, the MLVDS receiver will act normally and the output signal will not violate the mask, as shown in Figure 5. So the higher the noise immunity level, the more robust the device.

Figure 5: Noise immunity mask test with noise injection (mask nonviolation)

Noise will degrade MLVDS signals and negatively impact the performance of the whole system. Noise is pervasive in any application system. The noise source depends on the environment around the network. It may originate from noisy power supplies, high-current machinery, radio-frequency coupling, accidental electrostatic discharge (ESD) transients or other sources.

One commonly overlooked noise source is ESD transients that occur elsewhere in the system but translate into a noise source for MLVDS devices. MLVDS devices with higher noise immunity can suppress external noise more effectively, including ESD noise.

TI noise immunity performance vs. competitors

Figures 6 and 7 compare the noise immunity performance of TI’s SN65MLVD204B and SN65MLVD206B MLVDS transceivers vs. competing devices, respectively. The input clock for all noise immunity measurements is 25MHz. As the figures show, TI’s MLVDS solutions have higher noise immunity than its competitors and offer better stability against external noise sources, including ESD transients.

Figure 6: TI’s SN65MLVD204B vs. competing devices

Figure 7: TI’s SN65MLVD206B vs. competing devices

In conclusion, higher noise immunity of MLVDS devices means being able to suppress more noise in wired communication, optical communication and backplane applications, which makes sure that they are working properly.

For more information about the SN65MLVDS204B, SN65MLVDS206B and other TI MLVDS solutions, see www.ti.com/lvds or our TI E2E™ forum.