Related Posts
  • Blog Post: Cable equalization 101 – Automating your design

    Judging by the number of views on a post related to numerical cable equalization , on the High Speed E2E forum (more than 3,700 at last count!), I would guess that it’s a pretty interesting topic for many folks. Since TI is one of the leading manufacturers of current feedback amplifiers (CFA),...
  • Blog Post: Filter for thought

    Have you ever wondered how engineers designed active filters before the birth of software? They were able to do it using nomographs - but before we talk about what these are, let’s refresh our memory a little bit on active filters. Magnitude is the amplitude of the output. Phase is the angle...
  • Blog Post: Let’s take this driver out for a spin

    Before I suggest a suitable op amp to drive an ADC, I look at the application. This steers me toward one of two categories: low voltage or high voltage. If the system requires a low voltage operation, chances are I’ll look for a low power op amp. Depending on how low the power needs to be, I...
  • Blog Post: Being negative can still be positive

    The first operational amplifiers (op amps) used what is commonly called split power supplies, meaning the power for the amplifier was symmetrical around ground with both positive and negative polarities. Since most power supplies used transformers to convert 120 V mains electricity, a simple center tapped...
  • Blog Post: Supercapacitors to the rescue

    Monitoring the charging current of a supercapacitor application is very important. Without a precision current limiter, the charging current can overshoot when the voltage of the supercapacitor charges quickly, thus damaging the system. To prevent this, try this method to precisely limit the charging...
  • Blog Post: IAC or DIY? No, these aren’t stock tips!

    IAC is what I call integrated analog circuits, some prefer AFE (analog front ends) while others would say IS (integrated solutions.) Whereas DIY has a universal meaning, “do it yourself!” So the question now is, are you better off with an IAC over DIY, and why? It depends on the application...
  • Blog Post: Analog basics: Beginner knowledge and veteran refresher

    As a former college instructor who regularly lulled his students to sleep with a traditional lecture format, I’m excited to announce that TI is offering a “Hands-On Analog Basics” workshop at Design West 2013 (April 22-25 in San Jose, Calif.) with our very own amplifier expert, Art...
  • Blog Post: How to improve the startup and stop behavior of ERM and LRA actuators

    Eccentric rotating mass motors (ERM) and linear resonant actuators (LRA) are commonly used in smartphone and tablet applications to provide tactile feedback through haptic effects . While there are many characteristics to consider when designing for haptic feel, one of the most noticeable traits to users...
  • Blog Post: Reducing amplifier power consumption for SAR ADC drivers

    As power consumption in SAR ADCs gets smaller with every new device generation, the limitation in power sensitive applications becomes the amplifier. So how do we reduce power consumption further? Before looking at possible solutions, let’s consider the reason behind the reduction in power consumption...
  • Blog Post: Versatile tools to simplify your designs

    In a world where electronics are moving to lower supply voltages, it is comforting to know there are still components around that can tolerate higher supply voltages specifically when it comes to operational amplifiers (op amps). Op amps are essential building blocks and the option to select a high...
  • Blog Post: Introduction to the programmable differential amplifier

    Facing more complex systems and shorter design cycles than ever, designers need high performance components that are also flexible. Finding products that provide the best of both has always been a challenge. But, TI recently introduced the industry’s first programmable differential amplifier (PDA...
  • Blog Post: High-gain, high-bandwidth....putting it all together

    Over the last couple weeks we’ve covered how to achieve high-gain and high-bandwidth simultaneously as well as the implementation and what can go wrong. Here we will review how to put it all together. As simulations are only proof of concepts and should be considered with caution, I decided...
  • Blog Post: Engineer it: How to avoid electrical overstress of analog integrated circuits

    Have you had a chance to check out any videos from Engineer It ? We launched this series in 2012 as one more way to deliver in-depth advice on designs―directly from our experts. Scroll through the list on ti.com/engineerit to see what topics could be most helpful to you. We have everything from suggestions...
  • Blog Post: How to properly terminate an unused op amp

    We are often tasked by customers to select the best products to complete a design, including how to configure unused operational amplifiers in quad or dual op amp devices. While this may seem like a simple question to some, there are subtle aspects of operational amplifier behavior that must be understood...
  • Blog Post: Monthly Roundup: June

    Here are the top TI signal chain links in media coverage, awards and technical articles for the month of June. There is a nice mix of technical information spanning the signal chain to help you with your project – enjoy! Analog “ Analog: back to the future, part one ,” EDN...
  • Blog Post: Monthly Roundup: May

    Here are the top TI signal chain links in media coverage, awards and technical articles for the month of May. This was a great month for application notes, so it’s almost a guarantee you can find something of interest in the links below. Amplifiers "Harmonic Distortion: Part II...
  • Blog Post: Our demo offerings for Mobile World Congress

    Mobile World Congress is less than a week away, our demos have been shipped to Barcelona, and our team will soon be packing their suitcases for the flight to Spain (we bet someone will forget their toothbrush). We’re excited to have even more analog demos at this year’s show in applications...