Analog Wire
Tags
amplifiers and linear
analog
audio codec
Automotive & Transportation
Computing & Multimedia
DRV2605
DRV8662
Ebook
EMI
erm
ESD
haptic feedback
haptics
interface
lra
motor haptic driver
semiconductor
smartphone
Tablet
temperature sensor
texas instruments
ti
touch
touch screen
touch screen controller
Related Posts
Blog Post:
How to improve the startup and stop behavior of ERM and LRA actuators
Brian Burk
Eccentric rotating mass motors (ERM) and linear resonant actuators (LRA) are commonly used in smartphone and tablet applications to provide tactile feedback through haptic effects . While there are many characteristics to consider when designing for haptic feel, one of the most noticeable traits to users...
on
Apr 2, 2013
Blog Post:
Our new tablet and eBook solution guide is available now
Robert Rich
There's no question that tablets and eBooks are major players in today's consumer electronics industry, and manufacturers are working hard to come up with new functionalities and features to entice users. TI's new tablet and eBook solution guide provides a comprehensive reference guide...
on
Sep 14, 2011
Blog Post:
Enabling high-definition haptics: introducing piezo actuators
Eric.Siegel
Tactile feedback effects (commonly referred to as haptics) are an increasingly important component of both consumer and industrial applications, especially as touch screens become more prevalent. Users love touch screens, but they also love the feedback and satisfaction they get from pushing a physical...
on
Jul 25, 2011