Have you ever had the need to scavenge through multiple pages of a website just to locate a simple code example or documentation? MSP430ware is designed to answer that question. MSP430ware is a collection of all MSP430 user’s guide, datasheet, code examples, and many more in a simple navigational page. It also contains a driver library which can be used to initialize and utilize any peripherals on all MSP430F5xx and 6xx devices in an API form. Software developers now do not need to worry about low-level register details on what is needed to initialize a peripheral. MSP430ware also contains a collection of information and user experience code on several MSP430 tools. This allows customers to easily re-program or modify their experimenter board without searching through the web. This software is fully integrated into Code Composer Studio v5.1 and above with ease-of-use in mind. MSP430ware can also function as a standalone tool.
Visit www.ti.com/msp430ware for more information.
Regards,
William Goh
MSP430 Applications