The Official MSP430 Blog

  • You may have even seen it as 1 of 10 Cool Connected Watches in Forbes ! You might have even checked out some of the coolest applications it has inspired. It is back by popular demand and is the eZ430-Chonos , a wireless development tool in a watch! ...
  • In week one we brought you the MSP430 LaunchPad . In week two we brought you the SA430 spectrum analyzer . Now it's time to complete your wireless project with a development platform with a highly integrated, wearable wireless development system based...
  • Last week you got the MSP430 LaunchPad . So what's next? Maybe you want to add the Anaren Air BoosterPack and use a Chronos (hint, hint) for remote control . Either way this week's deal can definitely help you get started. This week we are offering...
  • It is the holiday season and we thought bringing you one last deal would be a great way to end the year! For the next 2 weeks we are offering 54% off of the following kits using the "MSP_Holiday" coupon code. eZ430-CHRONOS-868 (868 MHz...
  • Not long ago, we brought you a post on The Invisible Technology , describing multiple routes to enabling the Internet of Things in your applications, no matter what architecture you employ. One type of architecture that helps you keep things simple is...
  • In the past 3 weeks, we gave you everything you need to jumpstart wireless development with deals featuring the MSP430 LaunchPad , the SA430 spectrum analyzer and the eZ430-Chronos . To conclude our Back to School Sale we are bringing you a full wireless...
  • Introducing a cool new wearable development kit from InvenSense® featuring MSP430F5528 ULP technology: this 16bit, 128K flash MCU is used to control an InvenSense MPU-9150, 9-axis sensor and also provides USB or Bluetooth connectivity back to a host...
  • Want a new MSP430 tool for your next school project or just looking to take on another project for fun? Every Monday for the next 4 weeks , we will offer a surprise deal to help you get started! So what can you get this week? While supplies last the...
  • Need low power AND wireless communications in your application? We have the perfect tool for you! Jump start your design with this eZ430 platform from MSP430 and the CC2500 2.4 GHz transceiver . The eZ430-RF2500-SEH also comes with a solar panel to...
  • Are you saving up for that guitar tuner...that costs more than your guitar? Thanks to the MSP430 platform, you no longer have to! Our friend Andy was able to make his own stroboscopic guitar tuner for a fraction of the cost. For those of you new digital...

The Official MSP430 blog is a part of the TI Blogs and shares insights, behind-the-scenes news, deals and community projects related to ultra-low power microcontrollers (MCU) and applications. Make sure to sign up for email alerts or check back regularly for our latest ultra-low power content!