Welcome to the Blogs section of the TI E2E Community! Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers on TI’s Engineer-to-Engineer (E2E) Community
Over the last decade Unmanned Aerial Vehicles (UAV) have finally evolved from lab testing to field proven technologies. In a recent study, the Teal Group estimated overall UAV expenditures will double within a decade from $5.9 billion annually to $11.3 billion, with more than $94 billion spent over the next 10 years. Though the largest use base is still in the military, UAVs are now being used to provide surveillance for public safety and border control, fire fighting, traffic monitoring and potentially commercial communications.
Multicore processors, such as TI’s TMS320C6678 are particularly well suited for UAVs that are severely challenged by space constraints, power limitations and hot spot considerations (in some cases, the total power budget for a UAV can be sub 200 Watts). Through the use of multicore DSPs designers are still able to integrate a vast array of subsystems, including radar for target acquisition, image processing, a multitude of sensors, wideband and encrypted radio communications, powerful computer processing for mission analysis systems, video cameras and compression algorithms to store video data onboard the aircraft and many others.
The requirements for each of these functions in Unmanned Aircraft Systems seems to be growing in terms of performance within the same power footprint. For example, imaging systems on board the UAVs are going from 10 megapixel to several hundred mega pixels relying on power-efficient fixed and floating point devices such as our C6678 that run at under 10 Watts for an 8 core device running at 1GHz each.
What designers seem to especially like about our C66x multicore DSP portfolio is the scalability in aggregating multiple functions through DSP cores and acceleration, and the pin compatible 2,4 & 8 core devices that scale across a large power budget range.
I’d love to hear your thoughts on where this market is going. Are the recent defense cuts going to help or hinder the growth of such equipment? What are other considerations when designing such systems?