What Santa Didn’t Bring Me – and Why I’m Glad
On the fringe
RSS for posts
RSS for comments
Tweet
What Santa Didn’t Bring Me – and Why I’m Glad
Michael Sandoval
Feb 06 2008 18:35 PM
Comments
0
Gene Frantz
TI Principal Fellow and Business Development Manager, DSP
It’s been a couple of weeks since Christmas and my exploration of potential new toys at the Consumer Electronics Show, so I’ve had time to reflect on whether there were any big misses on my Christmas list and things I should be adding to next year’s list. I thought you might indulge me documenting this for future reference, so here goes.
One of the downsides of living with the “lunatic fringe” is that there are seldom surprises, specifically at CES. And for that matter, there are very few new “adult” gadgets (i.e., new computer, communications and entertainment products) that surprise me at Christmas. This isn’t a bad thing and shouldn’t get in the way of getting one or more of these wonderful new electronic toys to play with for Christmas. What this does mean is that I have to tell Santa exactly what I want – and sometimes I even have to purchase it myself, a phenomenon I’m sure many of you are familiar with.
So, what were some of my top choices this year? I’m certain I’ve forgotten a game or two, but there are several choices to think about:
A new home computer
A 1080p projector for my home theater
A Blue-ray DVD player (or is that a HD DVD player?)
Pleo
Yet another big screen TV
An upgrade on my PDA
A better digital still camera
So from this list, what did Santa get me? I got a new computer and a new digital still camera. The computer, which I needed, was like getting new underwear as a kid. My old computer, for some reason, lost use of the USB ports (I had been waiting for several years for something to “break” so I could justify buying a new one). With perfect timing, it broke just before Christmas, just in time to show up on my wish list. After my daughter and I discussed the choices, the details were given to Santa (if you haven’t guessed by now, Santa, at my house, is my wife – beautiful redhead without a beard). It arrived Christmas Eve, and I signed for it. We didn’t even wrap it.
The digital still camera I received is pretty nice, but since we have at least two other perfectly good cameras, confusion has now set in as to which one to use. Also, the twelve megapixels on the new camera somehow seems a little too much for my everyday attempt at photography. The good news is that my new camera is a Kodak and works on the same printer that our previous two Kodak cameras used.
So, with what I got in mind, what didn’t I get? And why is that a good thing?
Let me start with the whole 1080p thing. I have a 12-foot screen in my home theater, and I am still projecting SD media through a 480i projector. You know, this is OK because no one except me can tell that the picture is “poor” quality. This makes it very hard to convince Santa that I should pay $5000 for a new projector, then pay more for an HD DVD (or is that Blue Ray) DVD player and then pay even more for the media to play on it – that is, if the media is available. So, I am glad I didn’t get it this year. I’m a patient man – it will all be better and cheaper next year (This is the same excuse I used while our children were growing up to wait on buying a video camera; and, yes, we have no videos of their younger years).
I’ll note that at the CES, I didn’t see any breakthroughs to excite me into buying this year and perhaps not even for next Christmas. I wasn’t overly impressed with the 150-inch plasma TV set I saw – gee, I have about that same size screen hanging on the wall in my home theater and it didn’t cost a fortune. A cool thing I did see was the new 3D ready DLP TVs. This capability can be used in two ways: The obvious one is 3DTV when it is available and, not so obvious, dual TV. With dual TV, two people can be watching two different shows on the same TV on the full screen. It also sounds really great for gaming. Interesting, I didn’t ask if the audio channels were also capable of being split, but I assume that has been taken care of – or will be shortly.
So, I think I have covered everything except a new Mobile Internet Devices (do we still call them PDAs?) and Pleo. I’ll avoid talking about the MID and jump right to Pleo. Pleo is a new product on the market and is a robotic dinosaur – quite amazing. The company who makes Pleo is Ugobe, and they are doing some interesting stuff. I’m looking forward to see the second generation of Pleo which will hopefully have more TI content. Check them out here:
http://www.pleoworld.com/
.
It’s a good thing I collect baseball cards or it would have had a relatively quiet Christmas morning for me. But, I still have high hopes for next Christmas.
$core_v2_language.FormatString($ti.GetResource('Blog_PostQuestionAnswerView_CommentsCountFormatString'), $post.CommentCount)
lunatic fringe
,
gene frantz
,
CES
,
1080p
Sign in to Comment