How to Select a MOSFET – Switch Mode Power Supply


Perhaps the most common use for high-performance power MOSFETs in the current marketplace also presents the greatest challenge in selecting the most appropriate FET. Never are the trade-offs between performance, price and size more muddled than in the case with MOSFETs used in switch-mode power supplies (SMPSs).

Traversing an exhaustive list of SMPS topologies, both isolated and nonisolated, and listing the most important considerations for each would probably take a novel – and an applications expert with far more technical knowledge than a simple marketing engineer like me. But I do hope that in the proceeding paragraphs of this blog, I can offer at least a few tips and traps to avoid.

Most SMPS applications in today’s market operate at relatively high frequencies, from 100kHz all the way into the megahertz range. That means that unlike low-frequency applications like motor control, FET selection is not just about resistance and conduction losses. The higher the frequency, the greater the switching losses, which means that the best-performing or highest-efficiency FET is the one that best optimizes the trade-offs between low gate (and other) charges and low on-resistance, RDS(on).

Speaking of charges, it’s not all necessarily about gate charge either. The gate charge, QG, dictates the FET’s ability to turn on and off quickly, an important consideration for hard-switching applications where the faster the turn off, the less duration of voltage/current overlap. That is why the classic MOSFET silicon figure of merit (FOM) is RDS(ON) * QG, with the lowest value indicative of the best performance. But other switching parameters can be as – or more – important depending on the application. During high-side switching, stored energy losses, EOSS, dictated by output capacitance, COSS, can have a large impact on overall system efficiency (see Figure 1).

Figure 1: Power-loss breakdown of the control FET in a buck converter application

In order to achieve the higher efficiencies that contemporary power-supply energy standards demand, MOSFETs are replacing the sockets historically maintained by diodes to serve as synchronous rectifier switches (see Figure 2). For synchronous rectifier FETs, reverse-recovery losses dictated by the reverse-recovery charge of the MOSFET’s body diode, QRR, can often be the biggest contributors to power loss next to those conduction losses. For such applications, a more relevant FOM is RDS(ON) * (1/2 QOSS + QRR). Figure 3 shows a power-loss breakdown for an 80V MOSFET used in a typical synchronous rectification application.

Figure 2: In many applications, a low-resistance MOSFET replaces the rectifying diode to improve efficiency


Figure 3: Power-loss breakdown of a synchronous rectifier

Within a given FET technology for which respective FOMs are relatively equal, the lower the resistance, the higher the gate charge. Therefore, the most efficient solution is one that optimizes the respective contributions of both conduction and switching losses.

Consider a recent example in which a TI customer wanted a recommendation for a synchronous rectifier FET (for a given set of input conditions and specific output current). Figure 4 shows the respective conduction and switching losses for five different resistance FET options available. Note that the fourth and fifth options yielded very similar total power losses under these conditions, where the curve is more or less flat between the two. However, the fifth option is 2x the resistance of the fourth. Within a FET technology, resistance is inversely proportional to die size, so you can assume (correctly) that the fifth option is a significantly more cost-effective solution.

Figure 4: Power loss of five different MOSFET options – note that the fourth and fifth options have very similar total losses, although different conduction and switching losses

A few last points to consider:

  • It is not uncommon for an SMPS application to require a solution that parallels multiple FETs, particularly for synchronous rectifiers. Remember that differences in resistance between FET options will shrink by a factor proportional to the number of FETs you are paralleling. But at the same time, differences in charges will multiply by the same factor, such that at a certain number of FETs, the switching losses will work to decrease overall system efficiency.
  • Package selection matters as well. While older packages like transistor outline TO-220 and D2PAK can fit massive silicon die inside and dissipate large amounts of power (particularly through hole devices mounted to a large heat sink), they also have significantly higher package resistance than quad-flat no lead (QFN) devices. Also, at high frequencies, parasitic elements like the MOSFET’s source tab inductance begin to play a greater role and can have devastating impacts on switch-node ringing and overall system efficiency. Therefore, QFN packages (like TI’s SON5x6 or SON3x3) can achieve higher power density than their TO counterparts, and are almost always better suited for driving higher frequencies in the range of several hundred to a thousand kilohertz. That is why QFN packages like TI’s small outline no lead (SON) 5mm by 6mm or SON 3mm by 3mm can achieve higher power density than their TO counterparts, and are almost always better suited for driving higher frequencies in the range of several hundred to a thousand kilohertz.
  • You can discern some critical SMPS parameters, like RDS(on) and QG, straight from the MOSFET’s data sheet. Other parameters on the data sheet, like QRR and QOSS, are much more unreliable. Therefore, it is better to obtain an on-board, apples-to-apples measurement in order to get a fair comparison across different FET vendors.

If this post has only served to further muddy the waters and make the FET selection for SMPS applications appear more complicated than you previously thought, that was by design. FET selection is no trivial task and should not be treated as such. However, in the next installment of this series, I will discuss one extremely useful tool that TI has developed to make the selection of MOSFETs for one particular SMPS application – synchronous buck converters – as simple as plugging in a few parameters and analyzing the performance vs. cost trade-offs. Questions? Please feel free to leave a comment below.

 

  • Hi... I'm trying to create a high power SYNCHRONOUS rectifier BOOST converter to deliver 1000w and after many false starts, I'm currently focused on the TPS40360 which can cope with many paramaters of the design. Web Bench lets me have 53v @ 20amps output (from 20v in) BUT.. it cannot find suitable mosfets and having looked at a few 1000 (it feels) I can see why.. none have the right combination of LOW RDS and LOW gate charge for the current I need.  I'm struggling to find something in the very low Cgs arena which also has appropriate low RDS.  The closest potential FET is IPT015N10N5  which has a wonderfully low Rds but a horrifically high Cgs(tot) of 168 nC and when I relate this back to the DRIVER sections of the 43060..which have source and sink R of  2R Source and 1.8R sink.  When I run this through some 'rise time' calculations it's a drama.

    The frequency from WebBench is 540khz and that's a half cycle time of just  1.8 us   So, I'm worried that Switching losses will be off the planet.

    SOLUTION? I then looked at some TO-220 OPTIMOS fets, and found an interesting one. IPP083N10N5 which has Rds of 8.4mR but an astonishing Cgs TOTAL of only 30nC!  I'm thinking if I parallel 2 of these, the Cgs total will still only be  60nC and the DRIVERS in the 43060 should be able to cope with that even at high frequency?

    IF..I could parallel up the TI fet.... IPT015N10N5  with 146 nC gate charge... that would then give about 290nC  and I think with a R source=2R  it might slow things down way too much. (I'm happy to be persuaded otherwise... so you can sell more fets to me)

    The only other way I can think of to solve this problem is to lower the FREQUENCY to give the limited gate drive of the 43060 time to work... but that will mean a bigger inductor... not a problem for me.

    If anyone has shared a similar struggle.. I'm happy to hear from them and listen to suggestions.    motronic.buying@gmail.com

    I'm Julian de Ross