Improving the thermal performance of a power module


A derating curve like the one shown in Figure 1 is an essential part of making a power module easy to use. With the derating curve, you can quickly see if the power module is rated to support your particular application’s requirements. In most cases, the derating curve shows the rated output current at various ambient temperatures. Operating below this line operates the power module within its temperature, power and/or current limits.

Figure 1 shows several derating curves for a MicroSiP power module, each for a different value of the junction-to-ambient thermal resistance, commonly known as ΘJA. Wouldn’t you choose the power module that produces the green curve, since it has the lowest ΘJA and the least derating?

Figure 1: Derating curve for the a MicroSiP power module

 

Actually, each curve in Figure 1 uses the same TPS82130 power module under the same operating conditions. Only the printed circuit board (PCB) layout and airflow have changed. You, the designer, choose which derating curve you get. This brings to light a key truth about power modules: their thermal performance, and thus their derating, is highly dependent on the application and usage of the device, which includes the PCB layout and system variables such as airflow.

Specifically, the red curve in Figure 1 is generated with the standard Joint Electronic Devices Engineering Council (JEDEC) PCB design. While JEDEC’s board definition is used to generate most thermal tables in device data sheets, the JEDEC board is not a very realistic type of board for final applications.

Figure 2 shows one difference, of many, between the JEDEC PCB and a more typical application PCB: the amount of copper connected to the device’s pins. The very small amount of copper (shown in purple) used in the JEDEC design yields unrealistically poor thermal performance.

Figure 2: The JEDEC PCB uses very thin amounts of copper connecting to the device’s pins

By focusing on the thermal design when using a power module, it’s possible to easily achieve better performance than the JEDEC PCB. Table 1 shows several design options using different numbers of vias, layers and airflow. All are an improvement over the JEDEC PCB design, quantified by the lower ΘJA value and resulting lower operating temperature. Just through PCB and system design, you can reduce the operating temperature by nearly 50°C.

Table 1: Thermal-performance comparison of different PCB designs

Want to read more about this topic? Check out my article, “Improving the thermal performance of a MicroSiP power module,” in the Analog Design Journal.