George Lakkas
You can find hardware systems with multiple low-voltage rails that need regulation, sequencing and monitoring in cloud infrastructure equipment like base stations, networking switches, servers and storage, as well as test and measurement applications such as integrated circuit (IC) testers, oscilloscopes and network analyzers.
The Power Management Bus (PMBus) digital interface is a popular interface, which I discussed in another blog post, “A PMBus primer: common PMBus questions answered.”
TI has a complete PMBus power solution for systems using 48VDC on the front end and 12VDC or another low-voltage DC rail as the intermediate bus; see Figure 1.
The benefits of a complete PMBus solution in multirail systems are many: ease of use; reduced design time (as a new design can be generated in seconds by reconfiguring the on-chip nonvolatile memory [NVM]); reduction in overall component count and total solution cost; a unified and seamless design and programming method through a single graphical user interface (GUI); much simpler board characterization through PMBus margining; and improved diagnostics through voltage, current, temperature, power and fault monitoring.
Multirail PMBus sequencers/managers such as the 24-rail UCD90240 and the new 32-rail UCD90320 can sequence, margin, monitor and report faults for up to 32 rails using TI’s Fusion Digital Power™ GUI. They can also be stacked in fours for up to 128 rails, managed through the SYNC_CLK pin if needed.
Additionally, the UCD90240 and UCD90320 have true black-box logging that provides detailed information about all rails, General Purpose Input (GPI), and General Purpose Output (GPO) status on the first fault, as shown in Figure 2.
UCD90xxx PMBus sequencers/managers work with analog and PMBus point-of-load voltage regulators to provide a PMBus management and voltage-regulation solution in multirail systems, which almost always have one or more high-current application-specific integrated circuits (ASICs), processors and/or field-programmable gate arrays (FPGAs).
The loads require precise multiphase step-down conversion from the 12V intermediate bus to their respective rails. Typical load currents range from 50A to 200A, and the multiphase converter may require up to six phases to distribute power and thermals effectively and reduce the size and count of the inductor and output capacitors through phase interleaving.
One such six-phase converter is the TPS53667.
How does a multirail UCD90xxx PMBus sequencer come together with multiple PMBus voltage regulators in a design? The TI Designs PMBus Power System for Enterprise Ethernet Switches Reference Design is a good example, as shown in Figure 3.
The design employs a PMBus sequencer, a PMBus hot-swap IC (for the input current) and eight analog and PMBus voltage regulators, including a four-phase PMBus buck controller and a double-data-rate (DDR) termination (Vtt) switcher. The Fusion Digital Power GUI provides a graphical representation of the power tree and offers the capability to program the main parameters on the top half, while monitoring key parameters such as voltage, current, temperature and power on the bottom half.
If you are designing multirail systems with high-current processors, ASICs and/or FPGAs and want to simplify your design and characterization, reduce development time, and increase your system’s diagnostic capability, consider TI’s PMBus power solutions.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated