Technical solutions, industry trends and insights for designing and managing power supplies.
    • Dec 21, 2018

    Big things for power come in small packages

    Semiconductor packaging includes much more than just the material encapsulating the chip. While containing critical connections to the chip itself and to the circuit board, packaging technologies also include many innovations that help deliver the pe...
    • Dec 19, 2018

    Gallium nitride: supporting applications from watts to kilowatts

    Two years ago, TI announced its first 600-V gallium nitride (GaN) power device, which paved the way for engineers not only in power density and efficiency capability but also ease of design, with an integrated gate drive and robust device protection....
    • Dec 5, 2018

    Improving data-center efficiency with eFuses

    According to Forbes, global data centers used approximately 416TW (4.16 × 1014W) of electricity in 2017, with U.S. data centers contributing about 90 billion kilowatt hours to that number. With artificial intelligence making strides and 5G arou...
    • Dec 4, 2018

    How to use a voltage reference as a voltage regulator

    A version of this post was also published on Electronic Design . Have you ever needed to bias a low-current load and simply didn’t want to add another voltage regulator? Or been in a situation where you need a reasonable level of voltage accurac...
    • Nov 27, 2018

    Using an RGBW LED driver to elevate LED human-machine interface designs

    Products are becoming very intelligent and connected with each other. Devices such as speakers , TVs, refrigerators, set-top boxes and smoke detectors are no longer objects that just sit there – users can control them remotely or through voice ...
    • Nov 26, 2018

    QFN soldering tips and tricks

    If you’re looking to power a space-constrained, high-power-density, thermally critical application, high-efficiency converters in tiny quad flat no-lead (QFN) packages offer great performance value. But you might ask yourself, when you test and...
    • Nov 12, 2018

    How to add hysteresis to a DC/DC converter

    A version of this post was also published on Electronic Design . Is enable hysteresis not included in the DC/DC converter you are designing with? Or is the built-in enable hysteresis too small? Modern DC/DC converters use an enable pin to control the ...
    • Nov 8, 2018

    20 million reasons to use GaN

    It was a cold and snowy day in Toronto. We were brainstorming in the basement of the local university’s advanced power electronics research lab. Ironically, the conversation was focused on heat – not actually generating it for warmth, but how to reduce it in our power converters. We had pushed MOSFETs and IGBTs to their respective limits...
    • Nov 5, 2018

    How to speed SSD program time with a boost converter

    Solid-state drive (SSD) storage is becoming more popular in PC, data-center and telecom applications, offering the benefits of faster speeds and a more compact size compared to Hard Disk Drive (HDDs). The new Peripheral Component Interconnect Express...
    • Nov 1, 2018

    Delivering a smooth transition from AC to PoE power

    As the number of interconnected devices in the electronics market continues to grow, it becomes increasingly important to ensure interconnectivity between data-sensitive end equipment like wireless access points (WAPs), Internet Protocol (IP) camera...