Smart Grid
Tags
energy harvesting
Moore's Law
power efficiency
PV
solar
Related Posts
Blog Post:
Drawing a parallel between the Photovoltaic and the Semiconductor industry based on Moore’s Law
Nagarajan Sridhar
It is no surprise that the birth of the semiconductor chip (IC) industry has boosted technology and manufacturing to a large extent in the photovoltaic (PV) industry. Both of them use single crystal silicon wafers (to a large extent for now in the PV industry) and fabrication techniques and tools that...
on
Jun 28, 2010
Blog Post:
Solar energy storage for utility and harvesting applications
Nagarajan Sridhar
Capturing the energy from the sun and transferring it to electrical or thermal energy can be used to its fullest potential only if it can be stored. On a cloudy or rainy day or at night, energy needs to be provided to the consumer at any given time or on a continual basis. For this, storage technology...
on
May 8, 2009
Blog Post:
Band-gap engineering in photovoltaics: a simple yet challenging concept
Nagarajan Sridhar
Have you ever thought about how a solar cell functions and operates? Its function is quite simple: converting sunlight to electricity. Its operation is quite rudimentary. Solar cell is a semiconductor. The primary characteristic of a semiconductor is the presence of a band-gap . This band-gap has a finite...
on
Apr 16, 2009
Blog Post:
Solar Week March 9-13
PaulWestbrook
When people talk of solar power efficiency they are almost always referring to the conversion efficiency of the photovoltaic (PV) panel. The PV conversion efficiency is the ability to turn available sunlight into a DC voltage and current. For most mass produced panels the efficiency number is in the...
on
Mar 11, 2009