Related Posts
  • Blog Post: Grounding Principles

    In a previous blog on supply bypassing , I cautioned that poor bypassing could increase distortion of an amplifier. A reader, Walter, asked an interesting question… where should you connect the ground of a bypass capacitor to avoid problems? This raises questions regarding proper grounding...
  • Blog Post: Handy Gadgets and Resistor Divider Calculations

    Handy gadgets make our engineering life easier—the little special purpose computer programs or spreadsheets that you might find or create yourself. Back in the old days, engineers used nomographs. These are graphical aids that solve common multivariable problems of all sorts. Calculators and...
  • Blog Post: Chopper Op Amps—are they really noisy?

    Chopper op amps offer very low offset voltage and dramatically reduce low frequency 1/f (flicker) noise. How do they do it? Here’s a quick-read on the tricks. Click Here to read on EDN Magazine site.
  • Blog Post: Bypass Capacitors… yes, but why?

    Everyone knows that op amps should have power supply bypass capacitors located near the IC’s terminals, right? But why? Why, for example, is an amplifier more apt to oscillate without proper bypassing? The reasons will increase your understanding and awareness. Power supply rejection is an amplifier’s...
  • Blog Post: Rail-to-Rail Inputs—what you should know!

    Rail-to-Rail (R/R) op amps are extremely popular, especially useful with low supply voltage. You should know how R/R inputs are accomplished and understand some trade-offs. Figure 1 shows a typical dual-input R/R stage comprised of both N and P-channel transistor pairs. The P-channel FETs handle the...
  • Blog Post: Op Amps… G=1 stable & decompensated

    You have voted. Unity-gain-stable op amps won in a landslide—they’re far more popular than decompensated op amps. What’s this all about? Click Here to read on EDN Magazine site.
  • Blog Post: Paralleling Op Amps—is it possible?

    Is it possible to parallel two op amps to get twice the output current? We get this question periodically on our E2E forums. Though we may answer with a qualified “yes,” it tends to make us shudder just a bit. It can be done… but with great care. So let me come quickly to a key...
  • Blog Post: Resistor Puzzle—the sequel

    It’s time for some fun! I’ve known a few folks who have tormented colleagues with a resistor cube—equal resistors on all sides. So in case you’ve solved that one, let’s add a twist. In this cube, not all the resistors are equal. The resistance from A to B is 1Ω. Resistor...
  • Blog Post: 1/f Noise—the flickering candle

    The 1/f (one-over-f) low frequency noise region of amplifiers seems just a bit mysterious. Reader “tweet” asked for a discussion of 1/f noise—a challenging topic for a short blog. Click Here to read on EDN magazine web site. Excel noise calculation file here… (Please visit...
  • Blog Post: Simulating Gain-Bandwidth—the generic op amp model

    It may not always be obvious how the gain-bandwidth product (GBW) of an op amp may affect your circuits. Macro-models have a fixed GBW. Though you can look inside these models, it’s best not to tinker with them. What to do? You can use a generic op amp model in SPICE to check your circuits for...
  • Blog Post: ESD… Zapp!

    We’ve included device-level ESD performance of our ICs in data sheets for many years. But these figures apply to an integrated circuit before soldering onto your circuit board. What about ESD tolerance on your PCB ? We qualify the ESD performance by zapping each pin multiple times on several...
  • Blog Post: Op Amp Noise—but what about the feedback?

    Last month we explored noise of the non-inverting amplifier but I dodged the issue of the feedback network’s noise contribution. A reader, Jim, challenged me—he wanted more detail. So what about the noise from the feedback network? Click Here to read on EDN magazine web site. Excel...
  • Blog Post: The Inverting Attenuator, G = -0.1… is it unstable?

    Unity-gain-stable op amps are stable in a gain of one or greater, but not less, right? What to do? This question appears on our E2E forums periodically. Okay, here’s the short answer… an inverting attenuator is stable! You want to know why, right? There are a couple of ways to look...
  • Blog Post: Put Gain Up Front—waxing philosophical

    Low noise, low offset voltage, low drift—all the precision low-level signal processing goals get easier when you put voltage gain up front in the signal chain. It’s a simple concept. The error in the second stage is divided by the gain of the first stage, figure 1. For example, with only...
  • Blog Post: Input Capacitance—common-mode?...differential?… huh?

    The input capacitance specifications of op amps are often confused or ignored. Let’s clarify how these specs can best be used. Stability of an op amp circuit can be affected by input capacitance at the inverting input by causing phase shift—a delay of the feedback reaching the inverting...
  • Blog Post: Op Amp Noise—the non-inverting amplifier

    Building on last month's discussion of resistor noise, let’s check out some basics of amplifier noise. The non-inverting op amp configuration is most common for low noise applications so we’ll make that the focus. Click Here to read on EDN magazine web site. Other interesting...
  • Blog Post: Holiday Brain Teaser

    Here’s a little resistor puzzle to keep your mind sharp over the holidays. What is the resistance of this infinite resistor network? This can be solved numerically (and very accurately) but for this puzzle that’s considered cheating. Find the closed-form solution . And another challenge...
  • Blog Post: Breadboarding with Micro-Packages—Ouch!

    Have you noticed?...it’s rare to find new generation op amps and other ICs in DIPs (dual-inline packages). Without volume demand, it’s not economically viable to offer new ICs in DIPs. Breadboarding with these newer fine-pitch micro-packages can be a pain. What to do? This DIP adapter...
  • Blog Post: PCB Layout Tricks—striped capacitors and more

    I posed a question a couple of weeks ago regarding film capacitors—what’s the meaning of the stripe on one end? Check the picture below. These are non-polarized capacitors so it’s not a polarity marking. A reader, Richard, answered correctly—it identifies the outside conductive...
  • Blog Post: Resistor Noise—reviewing basics, plus a Fun Quiz

    The noise performance of amplifier circuits is greatly affected by the Johnson noise of resistors—the source resistance and feedback resistors. Most everyone seems to know that resistors have noise but may be a bit foggy on some of the details. Here’s a bite-sized review in preparation for...
  • Blog Post: The Unused Op Amp—what to do?

    I’m not referring to op amps in your parts bin. Those should be in anti-static bags or conductive foam. What about the one on your circuit board—the unused op amp in a quad or dual package. Hummm?? A recent question on our forums spurred me to address this subject but in the process, I...
  • Blog Post: Temperature Effects on Input Bias Current… plus a Random Quiz

    Last week we looked at the source of input bias current in CMOS and JFET amplifiers, finding that it comes from the leakage of one or more reverse-biased P-N junctions. Check it out if you missed it. We ended with a caution that these leakages increase significantly with temperature. The reverse-biased...
  • Blog Post: Input Bias Current of CMOS and JFET Amplifiers

    CMOS and JFET-input op amps are often selected for their low input bias current (I B ). But there is more to this than the single line in the spec table—subtleties that you should be aware of. Click Here to read on EDN web site. Index to all The Signal blogs.
  • Blog Post: Matchy Matchy—how alike are dual op amps?

    Some circuits benefit when the characteristics of two more op amps are closely matched. So inside a dual or quad op package, how closely do their behaviors match? Hummm? The most common request on our precision amplifier E2E forum is for matching offset voltage and offset voltage temperature drift...
  • Blog Post: Controlling Volume—log pots

    Have you ever tried to use a linear potentiometer (pot) as a volume control? Yikes! The volume jumps up much too rapidly. It requires a safe-cracker’s touch to adjust the volume to quiet listening levels. Thus the logarithmic potentiometer . Our senses have extremely wide dynamic ranges. Our...