Tools Insider
Tags
AM1808
ARM9 Microprocessor
bios
C5000 Ultra Low Power DSP
C6000 High Performance DSP
C6000 High Performance Multicore DSP
c6748
CCS
Davinci Digital Media Processor
Eclipse
Integra DSP+ARM Processor
Linux
omapl138
Open Source
Sitara ARM Cortex-A8 &
software
tools
Related Posts
Blog Post:
Linux SDK for OMAP-L138 LCDK: First stop for easy Linux innovation
Asheesh Bhardwaj
Our new Linux software development kit (SDK) for OMAP-L138 DSP + ARM9™ processors enables Linux lovers and ARM® aficionados to quickly and easily program their devices — at no cost! TI’s Linux SDK for OMAP-138 DSP + ARM9 processors is optimized for the newly announced OMAP-L138...
on
Jun 11, 2012
Blog Post:
Out with the old, in with biometrics-powered access control
Asheesh Bhardwaj
You may have seen the news about our TMS320C6748 DSP development kit (read Kanika Carver’s blog post: Access Granted 007-Style! . Kanika makes a good point: Many of the access control applications of today, complete with fingerprint detection as well as iris and face recognition, sound like they...
on
Jun 7, 2012
Blog Post:
What is the difference between Code Composer Studio v4 and v5?
JohnS
You may have heard about Code Composer Studio v5 you are probably wondering "should I be using v5 instead of v4? And if so why didn't I receive it as an upgrade notification?" Code Composer Studio v5 is not a replacement for v4 at this time. Instead it is available as a limited release...
on
Nov 1, 2010