Related Posts
  • Blog Post: CCS v4 Project Templates

    Starting with CCS 4.2, the New Project wizard includes Project Templates which helps with the creation of ready-made projects. Templates essentially define the inputs and processes required to create a project for a particular device. The templates presented by CCS are based on matching criteria defined...
  • Blog Post: CCSv4 tips - New feature of the project wizard

    Today I needed to create a small project to test a board and was surprised by a nice improvement to the Project manager of CCS version 4.2.0 RC1. I started by creating a new project using the Project Wizard (menu File --> New --> CCS Project ) and completely forgot to enable DSP/BIOS 5.4x support...
  • Blog Post: What is the difference between Code Composer Studio v4 and v5?

    You may have heard about Code Composer Studio v5 you are probably wondering "should I be using v5 instead of v4? And if so why didn't I receive it as an upgrade notification?" Code Composer Studio v5 is not a replacement for v4 at this time. Instead it is available as a limited release...