Tools Insider
Tags
AM1808
bios
C5000 Ultra Low Power DSP
C6000 High Performance DSP
C6000 High Performance Multicore DSP
c6748
C6-Integra DSP+ARM Processor
CCS
Davinci Digital Media Processor
Linux
omapl138
Sitara ARM Cortex-A8 & ARM9 Microprocessor
software
tools
Related Posts
Blog Post:
Linux SDK for OMAP-L138 LCDK: First stop for easy Linux innovation
Asheesh Bhardwaj
Our new Linux software development kit (SDK) for OMAP-L138 DSP + ARM9™ processors enables Linux lovers and ARM® aficionados to quickly and easily program their devices — at no cost! TI’s Linux SDK for OMAP-138 DSP + ARM9 processors is optimized for the newly announced OMAP-L138...
on
Jun 11, 2012
Blog Post:
Out with the old, in with biometrics-powered access control
Asheesh Bhardwaj
You may have seen the news about our TMS320C6748 DSP development kit (read Kanika Carver’s blog post: Access Granted 007-Style! . Kanika makes a good point: Many of the access control applications of today, complete with fingerprint detection as well as iris and face recognition, sound like they...
on
Jun 7, 2012
Blog Post:
CCS v4 Project Templates
AartiG
Starting with CCS 4.2, the New Project wizard includes Project Templates which helps with the creation of ready-made projects. Templates essentially define the inputs and processes required to create a project for a particular device. The templates presented by CCS are based on matching criteria defined...
on
Jan 7, 2011
Blog Post:
CCSv4 tips - New feature of the project wizard
desouza
Today I needed to create a small project to test a board and was surprised by a nice improvement to the Project manager of CCS version 4.2.0 RC1. I started by creating a new project using the Project Wizard (menu File --> New --> CCS Project ) and completely forgot to enable DSP/BIOS 5.4x support...
on
Nov 30, 2010