Defines

TI_USCI_SPI_Regs.h File Reference

Provides definitons for the SPI Hardware abastraction layer (HAL). More...

Go to the source code of this file.

Defines

#define USCI_AB_MODULE   0
#define IO_SPI_CS   BIT7
#define IO_SPI_SDI   BIT0
#define IO_SPI_SDO   BIT1
#define IO_SPI_SCLK   BIT2
#define STE_PxIN   P2IN
#define STE_PxOUT   P2OUT
#define STE_PxDIR   P2DIR
#define STE_PxSEL   P2SEL
#define STE_PxREN   P2REN
#define SIMO_PxIN   P3IN
#define SIMO_PxOUT   P3OUT
#define SIMO_PxDIR   P3DIR
#define SIMO_PxSEL   P3SEL
#define SIMO_PxREN   P3REN
#define SOMI_PxIN   P3IN
#define SOMI_PxOUT   P3OUT
#define SOMI_PxDIR   P3DIR
#define SOMI_PxSEL   P3SEL
#define SOMI_PxREN   P3REN
#define CLK_PxIN   P3IN
#define CLK_PxOUT   P3OUT
#define CLK_PxDIR   P3DIR
#define CLK_PxSEL   P3SEL
#define CLK_PxREN   P3REN

Detailed Description

Provides definitons for the SPI Hardware abastraction layer (HAL).

Author:
Daniel Torres - Texas Instruments, Inc
Date:
November 2010
Version:
1.0 Initial version
Note:
Built with IAR for MSP430 Version: 5.10

Definition in file TI_USCI_SPI_Regs.h.