Defines | Functions

TLV_descriptors.h File Reference

This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430. More...

Go to the source code of this file.

Defines

#define __MSP430_HAS_TLV__
#define TLV_START   (0x1A08)
#define TLV_END   (0x1AFF)
#define TLV_LDTAG   (0x01)
#define TLV_PDTAG   (0x02)
#define TLV_Reserved1   (0x03)
#define TLV_Reserved2   (0x04)
#define TLV_BLANK   (0x05)
#define TLV_Reserved3   (0x06)
#define TLV_SERNUM   (0x07)
#define TLV_DIERECORD   (0x08)
#define TLV_ADCCAL   (0x10)
#define TLV_TAGEXT   (0xFE)
#define TLV_TAGEND   (0xFF)

Functions

void Get_TLV_info (unsigned char tag, unsigned char *length, unsigned int *data_address)

Detailed Description

This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430.

Author:
Texas Instruments, Inc
Date:
November 2010
Version:
1.0 Initial version
Note:
Built with IAR for MSP430 Version: 5.10

Definition in file TLV_descriptors.h.