Defines | Typedefs | Enumerations | Functions

data_flash.h File Reference

this file contains all the definitions of the battery pack More...

Go to the source code of this file.

Defines

#define NUMBER_OF_BQ_DEVICES   3
#define NUMBER_OF_CELLS   18
#define MAX_CELLS_NUMBER_IN_BQ   6
#define CELL_BALANCING_EN   1
#define ONE_MINUTE   60
#define dCOV_THRESHOLD   3700
#define dCOV_RECOVERY_THRESHOLD   3600
#define dCOV_TIME   5
#define dCUV_THRESHOLD   2000
#define dCUV_RECOVERY_THRESHOLD   2200
#define dCUV_TIME   5
#define dPACK_OVER_TEMP1   50
#define dPACK_OT_TIME1   2000
#define dPACK_OVER_TEMP2   50
#define dPACK_OT_TIME2   2000
#define dPACK_END_OF_CHARGE_VOLTAGE   (DWORD)dCOV_THRESHOLD*NUMBER_OF_CELLS
#define dCC_CV_QUAL_TIME   20
#define dPACK_END_OF_DISCHARGE_VOLTAGE   (DWORD)dCUV_THRESHOLD*NUMBER_OF_CELLS
#define dEND_OF_DISCHARGE_QUAL_TIME   20
#define dCHARGE_CURRENT   1100
#define dCHARGE_TAPER_CURRENT   300
#define dCHARGE_TAPER_TIME   (DWORD)240*ONE_MINUTE
#define dMAX_CHARGE_TIME   (DWORD)200*ONE_MINUTE
#define dFULL_DISCHARGE_CLEAR_VOLTS   dPACK_END_OF_DISCHARGE_VOLTAGE
#define dFULL_CHARGE_CLEAR_VOLTS   dPACK_END_OF_CHARGE_VOLTAGE
#define dDELTA_CHARGE_V   300
#define dCHARGE_DISCHARGE_TIME   (DWORD)5*ONE_MINUTE
#define dDELTA_DISCHARGE_V   200
#define dSOV_THRESHOLD   4200
#define dSOV_RECOVERY_THRESHOLD   3800
#define dSOV_TIME   3000
#define dCELL_IMBALANCE_FAIL_THRESHOLD   500
#define dCELL_IMBALANCE_FAIL_TIME   (DWORD)120*ONE_MINUTE
#define dBALANCE_TIME   (DWORD)1*ONE_MINUTE
#define dBALANCE_VOLTS_THRESHOLD   50
#define dMIN_BALANCE_VOLTS   dCUV_RECOVERY_THRESHOLD
#define dMAX_BALANCE_TIME   (DWORD)120*ONE_MINUTE

Typedefs

typedef enum PARAM_ID param_id_t
 Global defines .

Enumerations

enum  PARAM_ID {
  COV_THRESHOLD, COV_RECOVERY_THRESHOLD, COV_TIME, CUV_THRESHOLD,
  CUV_RECOVERY_THRESHOLD, CUV_TIME, PACK_OVER_TEMP1, PACK_OT_TIME1,
  PACK_OVER_TEMP2, PACK_OT_TIME2, PACK_END_OF_CHARGE_VOLTAGE, CC_CV_QUAL_TIME,
  PACK_END_OF_DISCHARGE_VOLTAGE, END_OF_DISCHARGE_QUAL_TIME, CHARGE_CURRENT, CHARGE_TAPER_CURRENT,
  CHARGE_TAPER_TIME, MAX_CHARGE_TIME, FULL_DISCHARGE_CLEAR_VOLTS, FULL_CHARGE_CLEAR_VOLTS,
  DELTA_CHARGE_V, CHARGE_DISCHARGE_TIME, DELTA_DISCHARGE_V, SOV_THRESHOLD,
  SOV_RECOVERY_THRESHOLD, SOV_TIME, CELL_IMBALANCE_FAIL_THRESHOLD, CELL_IMBALANCE_FAIL_TIME,
  BALANCE_TIME, BALANCE_VOLTS_THRESHOLD, MIN_BALANCE_VOLTS, MAX_BALANCE_TIME
}
 

Global defines .


Functions

unsigned short get_u16_value (param_id_t param_id)
 Global functions declaration .
unsigned long get_u32_value (param_id_t param_id)
 Function Name: get_u32_value.

Detailed Description

this file contains all the definitions of the battery pack

Author:
Daniel Torres - Texas Instruments, Inc
Date:
November 2010
Version:
1.0 Initial version
Note:
Built with IAR for MSP430 Version: 5.10

Definition in file data_flash.h.


Function Documentation

unsigned short get_u16_value ( param_id_t  param_id  ) 

Global functions declaration .

Global functions declaration .

Description : Reads the flash memory and returns the value of the parameter

Parameters:
parameters : battery pack parameter to be read
Returns:
Value : value of the specific battery parameter

Definition at line 134 of file data_flash.c.

unsigned long get_u32_value ( param_id_t  param_id  ) 

Function Name: get_u32_value.

Description : Reads the flash memory and returns the value of the parameter

Parameters:
parameters : battery pack parameter to be read
Returns:
Value : value of the specific battery parameter

Definition at line 148 of file data_flash.c.