| bq_pack.c [code] | This file contains all the definitions of the BQ76PL536 devices |
| bq_pack.h [code] | This file contains all the definitions of the BQ76PL536 devices |
| data_flash.c [code] | This file contains all the functions needed to access to the battery pack information stored in the MSP430 flash memory |
| data_flash.h [code] | This file contains all the definitions of the battery pack |
| defMSP430USB.h [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| descriptors.c [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| descriptors.h [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| dma.c [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| hal_macros.h [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| hal_pmm.c [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| hal_pmm.h [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| hal_UCS.c [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| hal_UCS.h [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| main.c [code] | This file contains the state machine fuctions and the console functions, It also contains the appliaction functions and interrupt service routines |
| main.h [code] | This file contains all the definitions of the functions declared in main.c. It also contains the global variables used in other modules |
| spi_if.c [code] | This file contains the SPI functions and the CRC calculation |
| spi_if.h [code] | This file contains the SPI fuctions |
| TI_IO_Regs.h [code] | Generic I/O ports register definition |
| TI_USCI_SPI_Regs.h [code] | Provides definitons for the SPI Hardware abastraction layer (HAL) |
| TI_USCI_UART_Regs.h [code] | Generic UART register definition |
| TLV.c [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| TLV_descriptors.h [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| types.h [code] | This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430 |
| UART.c [code] | This file contains all the required functions to send and receive data using the UART module |
| UART.h [code] | This file contains all the required functions to send and receive data using the UART module |
| usb.c [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| usb.h [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| usb_eventHandling.c [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| UsbCdc.c [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| UsbCdc.h [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| USBCDC_constructs.c [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| USBCDC_constructs.h [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| UsbIsr.c [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
| UsbIsr.h [code] | For more information on this file please refer to Programmer’s Guide: MSP430 USB API Stack for CDC/HID http://focus.ti.com/docs/prod/folders/print/msp430f5529.html#toolssoftware |
1.7.1