This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430. More...
Go to the source code of this file.
Functions | |
| void | SetVCore (unsigned char level) |
| void | SetVCoreUp (unsigned char level) |
| void | SetVCoreDown (unsigned char level) |
This file contains definitions for the Hardware Abstraction Layer (HAL) specifically created for the MSP430.
Definition in file hal_pmm.h.
| void SetVCore | ( | unsigned char | level | ) |
| void SetVCoreDown | ( | unsigned char | level | ) |
1.7.1