this file contains all the definitions of the battery pack More...
Go to the source code of this file.
Defines | |
| #define | NUMBER_OF_BQ_DEVICES 3 |
| Battery pack definition. | |
| #define | NUMBER_OF_CELLS 18 |
| #define | MAX_CELLS_NUMBER_IN_BQ 6 |
| #define | CELL_BALANCING_EN 1 |
| #define | ONE_MINUTE 60 |
| #define | dCOV_THRESHOLD 3700 |
| Battery pack information and threshold values. | |
| #define | dCOV_RECOVERY_THRESHOLD 3600 |
| #define | dCOV_TIME 5 |
| #define | dCUV_THRESHOLD 2000 |
| #define | dCUV_RECOVERY_THRESHOLD 2200 |
| #define | dCUV_TIME 5 |
| #define | dPACK_OVER_TEMP1 50 |
| #define | dPACK_OT_TIME1 2000 |
| #define | dPACK_OVER_TEMP2 50 |
| #define | dPACK_OT_TIME2 2000 |
| #define | dPACK_END_OF_CHARGE_VOLTAGE (DWORD)dCOV_THRESHOLD*NUMBER_OF_CELLS |
| #define | dCC_CV_QUAL_TIME 20 |
| #define | dPACK_END_OF_DISCHARGE_VOLTAGE (DWORD)dCUV_THRESHOLD*NUMBER_OF_CELLS |
| #define | dEND_OF_DISCHARGE_QUAL_TIME 20 |
| #define | dCHARGE_CURRENT 1100 |
| #define | dCHARGE_TAPER_CURRENT 300 |
| #define | dCHARGE_TAPER_TIME (DWORD)240*ONE_MINUTE |
| #define | dMAX_CHARGE_TIME (DWORD)200*ONE_MINUTE |
| #define | dFULL_DISCHARGE_CLEAR_VOLTS dPACK_END_OF_DISCHARGE_VOLTAGE |
| #define | dFULL_CHARGE_CLEAR_VOLTS dPACK_END_OF_CHARGE_VOLTAGE |
| #define | dDELTA_CHARGE_V 300 |
| #define | dCHARGE_DISCHARGE_TIME (DWORD)5*ONE_MINUTE |
| #define | dDELTA_DISCHARGE_V 200 |
| #define | dSOV_THRESHOLD 4200 |
| #define | dSOV_RECOVERY_THRESHOLD 3800 |
| #define | dSOV_TIME 3000 |
| #define | dCELL_IMBALANCE_FAIL_THRESHOLD 500 |
| #define | dCELL_IMBALANCE_FAIL_TIME (DWORD)120*ONE_MINUTE |
| #define | dBALANCE_TIME (DWORD)1*ONE_MINUTE |
| #define | dBALANCE_VOLTS_THRESHOLD 50 |
| #define | dMIN_BALANCE_VOLTS dCUV_RECOVERY_THRESHOLD |
| #define | dMAX_BALANCE_TIME (DWORD)120*ONE_MINUTE |
Typedefs | |
| typedef enum PARAM_ID | param_id_t |
| Global defines . | |
Enumerations | |
| enum | PARAM_ID { COV_THRESHOLD, COV_RECOVERY_THRESHOLD, COV_TIME, CUV_THRESHOLD, CUV_RECOVERY_THRESHOLD, CUV_TIME, PACK_OVER_TEMP1, PACK_OT_TIME1, PACK_OVER_TEMP2, PACK_OT_TIME2, PACK_END_OF_CHARGE_VOLTAGE, CC_CV_QUAL_TIME, PACK_END_OF_DISCHARGE_VOLTAGE, END_OF_DISCHARGE_QUAL_TIME, CHARGE_CURRENT, CHARGE_TAPER_CURRENT, CHARGE_TAPER_TIME, MAX_CHARGE_TIME, FULL_DISCHARGE_CLEAR_VOLTS, FULL_CHARGE_CLEAR_VOLTS, DELTA_CHARGE_V, CHARGE_DISCHARGE_TIME, DELTA_DISCHARGE_V, SOV_THRESHOLD, SOV_RECOVERY_THRESHOLD, SOV_TIME, CELL_IMBALANCE_FAIL_THRESHOLD, CELL_IMBALANCE_FAIL_TIME, BALANCE_TIME, BALANCE_VOLTS_THRESHOLD, MIN_BALANCE_VOLTS, MAX_BALANCE_TIME } |
Global defines . More... | |
Functions | |
| unsigned short | get_u16_value (param_id_t param_id) |
| Global functions declaration . | |
| unsigned long | get_u32_value (param_id_t param_id) |
| Function Name: get_u32_value. | |
this file contains all the definitions of the battery pack
Definition in file data_flash.h.
| typedef enum PARAM_ID param_id_t |
Global defines .
definition of the Parameters structure
| enum PARAM_ID |
Global defines .
definition of the Parameters structure
Definition at line 128 of file data_flash.h.
| unsigned short get_u16_value | ( | param_id_t | param_id | ) |
Global functions declaration .
Global functions declaration .
Description : Reads the flash memory and returns the value of the parameter
| parameters | : battery pack parameter to be read |
Definition at line 134 of file data_flash.c.
| unsigned long get_u32_value | ( | param_id_t | param_id | ) |
Function Name: get_u32_value.
Description : Reads the flash memory and returns the value of the parameter
| parameters | : battery pack parameter to be read |
Definition at line 148 of file data_flash.c.
1.7.1