Starting with version 7.40A of IAR Embedded Workbench for 8051, this driver was renamed to "Texas Instruments" in all IDE dialog boxes.
Support has been added for the CC2540 device family.
EW18593
It is not possible to set breakpoints when using preprocessed C source code with
#line statements unless you write the absolute path for the file e.g: #line 3 "c:\\path\\file.c"
Known problems that are common for all drivers are listed here.
EW22134
An issue was corrected that would cause the debugging session to be terminated abnormally when inspecting the contents of the Radio registers using either the register window, or the memory window.
Corrections that are common for all drivers are listed here.
V7.51A, April 2009
Support has been added for the CC25xx device family. The options dialog for this driver has also been modify to accomodate for the different mechanism used for protecting flash memory for these devices. Flash pages that are to be protected should be specifies as a string of decimal caracters, according to the example provided in the options dialog.
V7.50A, June 2008
No changes.
V7.40A, Feb 2008
No changes.
V7.30B, September 2007
An error was corrected that could cause a page being written to flash to partially overwrite a previously written page with garbage data.
7.21A, May 2007
Flash protection (boot block, debug inteface and page) added.
Retain memory pages added. Pages to be retined should be entered on the form 1,2,3,4....62,63. To retain IEEE address "IEEE" can be entered.
Mapping SFRs and XDATA to CODE memory when using unified memory access could sometimes cause inadvertent reads of registers that use hardware clearing.
7.20H, Nov 2007
Better support for the latest revision of CC2430.
The driver has been updated in order to improve overall stability.
The Chipcon driver dialog window has been updated with improved logic to handle checkbox options.
7.20D, May 2006
A new menu option, Leave target running, has been added in the Chipcon debug menu. Selecting this option will leave the target system running when the debug session is closed.
The FMAP register was erroneously overwritten when execution was stopped. This could cause problems if execution was stopped while running in an interrupt or library routine.
7.20C, January 2006
Smaller update of the debuggers has been done for this release. Most updates have been done to improve the stability and speed of the various debuggers.
7.20A, October 2005
Initial release.
Copyright 2006-2009 IAR Systems. All rights reserved.