csl_memprotAux.h File Reference

API Auxilary header file for MEMPROT CSL. Contains the different control command and status query functions definations. More...

#include <ti/csl/csl_memprot.h>

Functions

CSL_IDEF_INLINE Uint32 CSL_MEMPROT_getL2FaultAddress (void)
CSL_IDEF_INLINE void CSL_MEMPROT_clearL2Fault (void)
CSL_IDEF_INLINE void CSL_MEMPROT_getL2FaultStatus (CSL_MEMPROT_MPFSR *mpfsr)
CSL_IDEF_INLINE void CSL_MEMPROT_setL2Attributes (Uint32 index, CSL_MEMPROT_MPPA *mppa)
CSL_IDEF_INLINE void CSL_MEMPROT_getL2Attributes (Uint32 index, CSL_MEMPROT_MPPA *mppa)
CSL_IDEF_INLINE Uint32 CSL_MEMPROT_getL1PFaultAddress (void)
CSL_IDEF_INLINE void CSL_MEMPROT_clearL1PFault (void)
CSL_IDEF_INLINE void CSL_MEMPROT_getL1PFaultStatus (CSL_MEMPROT_MPFSR *mpfsr)
CSL_IDEF_INLINE void CSL_MEMPROT_setL1PAttributes (Uint32 index, CSL_MEMPROT_MPPA *mppa)
CSL_IDEF_INLINE void CSL_MEMPROT_getL1PAttributes (Uint32 index, CSL_MEMPROT_MPPA *mppa)
CSL_IDEF_INLINE Uint32 CSL_MEMPROT_getL1DFaultAddress (void)
CSL_IDEF_INLINE void CSL_MEMPROT_clearL1DFault (void)
CSL_IDEF_INLINE void CSL_MEMPROT_getL1DFaultStatus (CSL_MEMPROT_MPFSR *mpfsr)
CSL_IDEF_INLINE void CSL_MEMPROT_setL1DKey (Uint32 index, Uint32 l1dkey)
CSL_IDEF_INLINE void CSL_MEMPROT_resetL1DLock (void)
CSL_IDEF_INLINE void CSL_MEMPROT_lockL1D (void)
CSL_IDEF_INLINE void CSL_MEMPROT_unlockL1D (void)
CSL_IDEF_INLINE void CSL_MEMPROT_getL1DLockStatus (CSL_MEMPROT_MPLKSTAT *mplkstat)
CSL_IDEF_INLINE void CSL_MEMPROT_setL1DAttributes (Uint32 index, CSL_MEMPROT_MPPA *mppa)
CSL_IDEF_INLINE void CSL_MEMPROT_getL1DAttributes (Uint32 index, CSL_MEMPROT_MPPA *mppa)


Detailed Description

API Auxilary header file for MEMPROT CSL. Contains the different control command and status query functions definations.

============================================================================
(C) Copyright 2008, 2009, Texas Instruments, Inc.
Use of this software is controlled by the terms and conditions found
in the license agreement under which this software has been supplied. ===========================================================================

Copyright 2011, Texas Instruments Incorporated