csl_rac_regsGCCPAux.c File Reference

This file contains all the API operation prototypes for RAC COMMON CSL for the GCCP. More...

#include <ti/csl/csl_rac_regsGCCPAux.h>

Functions

void CSL_RAC_GCCP_enable (CSL_RAC_Handle hRac, Uint8 gccpId)
void CSL_RAC_GCCP_disable (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint16 CSL_RAC_GCCP_getActiveCycles (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint16 CSL_RAC_GCCP_getSequencerCycles (CSL_RAC_Handle hRac, Uint8 gccpId)
void CSL_RAC_GCCP_resetHighPriorityQueue (CSL_RAC_Handle hRac, Uint8 gccpId)
void CSL_RAC_GCCP_resetLowPriorityQueue (CSL_RAC_Handle hRac, Uint8 gccpId)
void CSL_RAC_GCCP_getReadTime (CSL_RAC_Handle hRac, CSL_RAC_FE_Timestamp_req *timestamp)
Uint32 CSL_RAC_GCCP_getLowPrioDataLevel (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint32 CSL_RAC_GCCP_getLowPrioDataWatermark (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint32 CSL_RAC_GCCP_getHighPrioDataLevel (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint32 CSL_RAC_GCCP_getHighPrioDataWatermark (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint32 CSL_RAC_GCCP_getLowPrioControlLevel (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint32 CSL_RAC_GCCP_getLowPrioControlWatermark (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint32 CSL_RAC_GCCP_getHighPrioControlLevel (CSL_RAC_Handle hRac, Uint8 gccpId)
Uint32 CSL_RAC_GCCP_getHighPrioControlWatermark (CSL_RAC_Handle hRac, Uint8 gccpId)
void CSL_RAC_GCCP_setIctEntry (CSL_RAC_Handle hRac, Uint8 gccpId, Uint8 entryId, Int8 coeff0, Int8 coeff1, Int8 coeff2, Int8 coeff3)
void CSL_RAC_GCCP_setCgtEntry (CSL_RAC_Handle hRac, Uint8 gccpId, Uint8 entryId, Uint32 partY)
Uint32 CSL_RAC_GCCP_getCgtEntry (CSL_RAC_Handle hRac, Uint8 gccpId, Uint8 entryId)
void CSL_RAC_GCCP_setPrtEntry (CSL_RAC_Handle hRac, Uint8 gccpId, Uint8 entryId, Uint8 wordId, Uint32 format)
Uint32 CSL_RAC_GCCP_getPrtEntry (CSL_RAC_Handle hRac, Uint8 gccpId, Uint8 entryId, Uint8 wordId)
void CSL_RAC_GCCP_getCycleOverflowStatus (CSL_RAC_Handle hRac, Uint8 gccpId, CSL_RAC_GCCP_cycleOverflowStatus *cycleOverflowStatus)
void CSL_RAC_GCCP_getFifoOverflowStatus (CSL_RAC_Handle hRac, Uint8 gccpId, CSL_RAC_GCCP_fifoOverflowStatus *fifoOverflowStatus)


Detailed Description

This file contains all the API operation prototypes for RAC COMMON CSL for the GCCP.

============================================================================
(C) Copyright 2002, 2003, 2004, 2005, 2006, Texas Instruments, Inc.
Use of this software is controlled by the terms and conditions found
in the license agreement under which this software has been supplied. ===========================================================================

Copyright 2011, Texas Instruments Incorporated