csl_tac_regsBEAux.c File Reference

This file contains API implementation for the CSL for the TAC Back-End interface. More...

#include <ti/csl/csl_tac_regsBEAux.h>

Functions

void CSL_TAC_BETI_enable ()
void CSL_TAC_BETI_disable ()
CSL_TAC_BETI_enableStatus CSL_TAC_BETI_getEnableStatus ()
void CSL_TAC_BETI_getStatus (CSL_TAC_BETI_status *betiStatus)
void CSL_TAC_BETI_setWatchDog (Uint16 reloadCnt)
Uint16 CSL_TAC_BETI_getWatchDogStatus ()
CSL_TAC_BETI_wdInterruptStatus CSL_TAC_BETI_getWatchDogInterruptStatus ()
void CSL_TAC_BETI_clearWatchDogInterrupt ()
void CSL_TAC_BEII_enable ()
void CSL_TAC_BEII_disable ()
CSL_TAC_BEII_enableStatus CSL_TAC_BEII_getEnableStatus ()
void CSL_TAC_BEII_getInterruptStatus (CSL_TAC_BEII_interruptStatus *interruptStatus)
void CSL_TAC_BEII_getEnabledInterruptStatus (CSL_TAC_BEII_interruptStatus *interruptEnStatus)
void CSL_TAC_BEII_forceInterrupts (CSL_TAC_BEII_interruptStatus *interruptsToForce)
void CSL_TAC_BEII_clearInterrupts (CSL_TAC_BEII_interruptStatus *interruptsToClear)
void CSL_TAC_BEII_enableInterrupts (CSL_TAC_BEII_interruptStatus *interruptsToEnable)
void CSL_TAC_BEII_disableInterrupts (CSL_TAC_BEII_interruptStatus *interruptsToDisable)
void CSL_TAC_BEII_setEOI (Uint32 eoiVecValue)
Uint32 CSL_TAC_BEII_getEOI ()
CSL_TAC_BE_strmPwrMeasMode CSL_TAC_BE_getStrmPwrMeasMode ()
void CSL_TAC_BE_setSwIterStart ()
void CSL_TAC_BE_setTimestamp (CSL_TAC_BE_Timestamp_req *timestamp)
void CSL_TAC_BE_getTimestamp (CSL_TAC_BE_Timestamp_req *timestamp)


Detailed Description

This file contains API implementation for the CSL for the TAC Back-End interface.

============================================================================

Date:
03-Feb-2009
Author:
Vijay Pothukuchi
============================================================================
(C) Copyright 2009, Texas Instruments, Inc.
Use of this software is controlled by the terms and conditions found
in the license agreement under which this software has been supplied. ===========================================================================

Copyright 2011, Texas Instruments Incorporated