csl_xmcAux.h File Reference

API Auxilary header file for XMC CSL. It gives the definitions of the status query & control functions. More...

#include <ti/csl/csl_xmc.h>

Functions

CSL_IDEF_INLINE void CSL_XMC_setXMPAXH (Uint32 index, CSL_XMC_XMPAXH *mpaxh)
CSL_IDEF_INLINE void CSL_XMC_setXMPAXL (Uint32 index, CSL_XMC_XMPAXL *mpaxl)
CSL_IDEF_INLINE void CSL_XMC_getXMPAXH (Uint32 index, CSL_XMC_XMPAXH *mpaxh)
CSL_IDEF_INLINE void CSL_XMC_getXMPAXL (Uint32 index, CSL_XMC_XMPAXL *mpaxl)
CSL_IDEF_INLINE Uint32 CSL_XMC_getFaultAddress (void)
CSL_IDEF_INLINE void CSL_XMC_clearFault (void)
CSL_IDEF_INLINE void CSL_XMC_getFaultStatus (CSL_XMC_MPFSR *xmpfsr)
CSL_IDEF_INLINE void CSL_XMC_invalidatePrefetchBuffer (void)
CSL_IDEF_INLINE void CSL_XMC_loadAnalysisCounterEnable (void)
CSL_IDEF_INLINE void CSL_XMC_setAnalysisCounterEnableMode (CSL_XMC_ACEN_MODE acenMode)
CSL_IDEF_INLINE void CSL_XMC_resetAnalysisCounters (void)
CSL_IDEF_INLINE void CSL_XMC_setPrefetchCommand (Uint8 inv, Uint8 acEnLoad, CSL_XMC_ACEN_MODE acenMode, Uint8 acRst)
CSL_IDEF_INLINE CSL_XMC_ACEN_MODE CSL_XMC_getAnalysisCounterEnableStatus (void)
CSL_IDEF_INLINE Uint32 CSL_XMC_getNumPrefetchSent (void)
CSL_IDEF_INLINE Uint32 CSL_XMC_getNumPrefetchCanceled (void)
CSL_IDEF_INLINE Uint32 CSL_XMC_getNumPrefetchHits (void)
CSL_IDEF_INLINE Uint32 CSL_XMC_getNumPrefetchMisses (void)
CSL_IDEF_INLINE void CSL_XMC_getPrefetchAddress (Uint32 index, CSL_XMC_XPFADDR *xpfaddr)
CSL_IDEF_INLINE void CSL_XMC_setMDMAPriority (Uint32 priority)
CSL_IDEF_INLINE Uint32 CSL_XMC_getMDMAPriority (void)


Detailed Description

API Auxilary header file for XMC CSL. It gives the definitions of the status query & control functions.

============================================================================
(C) Copyright 2008, 2009, Texas Instruments, Inc.
Use of this software is controlled by the terms and conditions found
in the license agreement under which this software has been supplied. ===========================================================================

Copyright 2011, Texas Instruments Incorporated