![]() |
![]() |
Typedefs | |
| typedef volatile CSL_CPINTCRegs * | CSL_CPINTC_RegsOvly |
| Register Overlay Memory map for the CPINTC0 Registers. | |
| typedef Uint32 | CSL_CPINTC_Handle |
| This is the handle to the CPINTC instance. | |
| typedef Uint32 | CSL_CPINTCSystemInterrupt |
| This defines the system interrupt. | |
| typedef Uint32 | CSL_CPINTCHostInterrupt |
| This defines the host interrupt. | |
| typedef Uint32 | CSL_CPINTCChannel |
| This defines the channels. | |
| typedef Uint16 | CSL_CPINTCNestingLevel |
| This defines the nesting level. | |
Enumerations | |
| enum | CSL_CPINTCNestingMode |
| Enumeration defines the type of Nesting Modes which is supported by the CPINTC. | |