CPSW_3GF Data Structures
[Ethernet switch submodule (CPSW_3GF)]


Data Structures

struct  CSL_CPSW_3GF_VERSION
 Holds the Time sync submodule's version info. More...
struct  CSL_CPSW_3GF_CONTROL
 Holds CPSW control register contents. More...
struct  CSL_CPSW_3GF_PORTSTAT
 Holds Port Statistics Enable register contents. More...
struct  CSL_CPSW_3GF_PTYPE
 Holds Priority type register contents. More...
struct  CSL_CPSW_3GF_FLOWCNTL
 Holds flow control register contents. More...
struct  CSL_CPSW_3GF_TSCNTL
 Holds Port Time Sync Control register contents. More...
struct  CSL_CPSW_3GF_STATS
 Holds the EMAC statistics. More...
struct  CSL_CPSW_3GF_ALE_VERSION
 Holds the ALE submodule's version info. More...
struct  CSL_CPSW_3GF_ALE_PORTCONTROL
 Holds the ALE Port control register info. More...
struct  CSL_CPSW_3GF_ALE_MCASTADDR_ENTRY
 Holds the ALE Multicast Address Table entry configuration. More...
struct  CSL_CPSW_3GF_ALE_VLANMCASTADDR_ENTRY
 Holds the ALE VLAN/Multicast Address Table entry configuration. More...
struct  CSL_CPSW_3GF_ALE_UNICASTADDR_ENTRY
 Holds the ALE Unicast Address Table entry configuration. More...
struct  CSL_CPSW_3GF_ALE_OUIADDR_ENTRY
 Holds the ALE OUI Unicast Address Table entry configuration. More...
struct  CSL_CPSW_3GF_ALE_VLANUNICASTADDR_ENTRY
 Holds the ALE VLAN Unicast Address Table entry configuration. More...
struct  CSL_CPSW_3GF_ALE_VLAN_ENTRY
 Holds the ALE VLAN Table entry configuration. More...

Defines

#define hCpsw3gfRegs   ((CSL_Cpsw_3gfRegs *) (CSL_PA_SS_CFG_REGS + 0x00090800))
 Pointer to the Ethernet Switch overlay registers.
#define CSL_CPSW_3GF_NUMSTATBLOCKS   2
 Number of statistic blocks.
#define CSL_CPSW_3GF_NUMSTATS   36
 Number of hardware statistics registers.
#define CSL_CPSW_3GF_NUMALE_ENTRIES   1024
 Maximum number of ALE entries that can be programmed.
#define CSL_CPSW_3GF_ALECONTROL_RATELIMIT_EN   (1 << 0u)
 ALE control register configuration definitions.
#define CSL_CPSW_3GF_ALECONTROL_AUTHMODE_EN   (1 << 1u)
#define CSL_CPSW_3GF_ALECONTROL_VLANAWARE_EN   (1 << 2u)
#define CSL_CPSW_3GF_ALECONTROL_RATELIMIT_TX_EN   (1 << 3u)
#define CSL_CPSW_3GF_ALECONTROL_OUIDENY_EN   (1 << 5u)
#define CSL_CPSW_3GF_ALECONTROL_VID0MODE_EN   (1 << 6u)
#define CSL_CPSW_3GF_ALECONTROL_LEARN_NO_VID_EN   (1 << 7u)
#define CSL_CPSW_3GF_ALECONTROL_AGEOUT_NOW_EN   (1 << 29u)
#define CSL_CPSW_3GF_ALECONTROL_CLRTABLE_EN   (1 << 30u)
#define CSL_CPSW_3GF_ALECONTROL_ALE_EN   (1 << 31u)
#define CSL_CPSW_3GF_PORTMASK_PORT0_EN   (1 << 0u)
 Port Mask definitions.
#define CSL_CPSW_3GF_PORTMASK_PORT1_EN   (1 << 1u)
#define CSL_CPSW_3GF_PORTMASK_PORT2_EN   (1 << 2u)

Enumerations

enum  CSL_CPSW_3GF_ALE_PORTSTATE
 Defines ALE port states.
enum  CSL_CPSW_3GF_ALE_ENTRYTYPE
 Defines ALE Table Entry types.
enum  CSL_CPSW_3GF_ALE_UCASTTYPE
 Defines ALE Unicast types.
enum  CSL_CPSW_3GF_ALE_ADDRTYPE
 Defines ALE Address types.

Define Documentation

#define CSL_CPSW_3GF_ALECONTROL_AGEOUT_NOW_EN   (1 << 29u)

Age out now enable

#define CSL_CPSW_3GF_ALECONTROL_ALE_EN   (1 << 31u)

ALE enable

#define CSL_CPSW_3GF_ALECONTROL_AUTHMODE_EN   (1 << 1u)

MAC auhorization mode enable

#define CSL_CPSW_3GF_ALECONTROL_CLRTABLE_EN   (1 << 30u)

Clear table enable

#define CSL_CPSW_3GF_ALECONTROL_LEARN_NO_VID_EN   (1 << 7u)

Learn no VID enable

#define CSL_CPSW_3GF_ALECONTROL_OUIDENY_EN   (1 << 5u)

OUI deny enable

#define CSL_CPSW_3GF_ALECONTROL_RATELIMIT_EN   (1 << 0u)

ALE control register configuration definitions.

Enable Broadcast/Multicast rate limit

#define CSL_CPSW_3GF_ALECONTROL_RATELIMIT_TX_EN   (1 << 3u)

Tx rate limit enable

#define CSL_CPSW_3GF_ALECONTROL_VID0MODE_EN   (1 << 6u)

VID0 mode enable

#define CSL_CPSW_3GF_ALECONTROL_VLANAWARE_EN   (1 << 2u)

VLAN Aware Mode enable

#define CSL_CPSW_3GF_NUMSTATBLOCKS   2

Number of statistic blocks.

EMAC has two sub-blocks: STATSA and STATSB.

STATSA holds statistics for Host/CPU port (Switch port 0). STATSB holds statistics for MAC ports (Switch ports 1, 2).

#define CSL_CPSW_3GF_PORTMASK_PORT0_EN   (1 << 0u)

Port Mask definitions.

Port 0 Enable

#define CSL_CPSW_3GF_PORTMASK_PORT1_EN   (1 << 1u)

Port 1 Enable

#define CSL_CPSW_3GF_PORTMASK_PORT2_EN   (1 << 2u)

Port 2 Enable


Copyright 2011, Texas Instruments Incorporated