EDMA3 Symbols Defined
[EDMA3]


Defines

#define CSL_EDMA3_REGION_GLOBAL   -1
#define CSL_EDMA3_LINK_NULL   0xFFFF
#define CSL_EDMA3_LINK_DEFAULT   0xFFFF
#define CSL_EDMA3_SYNC_A   0
#define CSL_EDMA3_SYNC_AB   1
#define CSL_EDMA3_TCC_NORMAL   0
#define CSL_EDMA3_TCC_EARLY   1
#define CSL_EDMA3_FIFOWIDTH_NONE   0
#define CSL_EDMA3_FIFOWIDTH_8BIT   0
#define CSL_EDMA3_FIFOWIDTH_16BIT   1
#define CSL_EDMA3_FIFOWIDTH_32BIT   2
#define CSL_EDMA3_FIFOWIDTH_64BIT   3
#define CSL_EDMA3_FIFOWIDTH_128BIT   4
#define CSL_EDMA3_FIFOWIDTH_256BIT   5
#define CSL_EDMA3_ADDRMODE_INCR   0
#define CSL_EDMA3_ADDRMODE_CONST   1
#define CSL_EDMA3_MEMACCESS_UX   0x0001
#define CSL_EDMA3_MEMACCESS_UW   0x0002
#define CSL_EDMA3_MEMACCESS_UR   0x0004
#define CSL_EDMA3_MEMACCESS_SX   0x0008
#define CSL_EDMA3_MEMACCESS_SW   0x0010
#define CSL_EDMA3_MEMACCESS_SR   0x0020
#define CSL_EDMA3_MEMACCESS_EXT   0x0200
#define CSL_EDMA3_MEMACCESS_AID0   0x0400
#define CSL_EDMA3_MEMACCESS_AID1   0x0800
#define CSL_EDMA3_MEMACCESS_AID2   0x1000
#define CSL_EDMA3_MEMACCESS_AID3   0x2000
#define CSL_EDMA3_MEMACCESS_AID4   0x4000
#define CSL_EDMA3_MEMACCESS_AID5   0x8000
#define CSL_EDMA3_ITCINT_EN   1
#define CSL_EDMA3_ITCINT_DIS   0
#define CSL_EDMA3_ITCCH_EN   1
#define CSL_EDMA3_ITCCH_DIS   0
#define CSL_EDMA3_TCINT_EN   1
#define CSL_EDMA3_TCINT_DIS   0
#define CSL_EDMA3_TCCH_EN   1
#define CSL_EDMA3_TCCH_DIS   0
#define CSL_EDMA3_STATIC_EN   1
#define CSL_EDMA3_STATIC_DIS   0
#define CSL_EDMA3_TRIGWORD_DEFAULT   7
#define CSL_EDMA3_TRIGWORD_OPT   0
#define CSL_EDMA3_TRIGWORD_SRC   1
#define CSL_EDMA3_TRIGWORD_A_B_CNT   2
#define CSL_EDMA3_TRIGWORD_DST   3
#define CSL_EDMA3_TRIGWORD_SRC_DST_BIDX   4
#define CSL_EDMA3_TRIGWORD_LINK_BCNTRLD   5
#define CSL_EDMA3_TRIGWORD_SRC_DST_CIDX   6
#define CSL_EDMA3_TRIGWORD_CCNT   7
#define CSL_EDMA3_OPT_MAKE(itcchEn, tcchEn, itcintEn, tcintEn, tcc, tccMode, fwid, stat, syncDim, dam, sam)
#define CSL_EDMA3_CNT_MAKE(aCnt, bCnt)
#define CSL_EDMA3_LINKBCNTRLD_MAKE(link, bCntRld)
#define CSL_EDMA3_BIDX_MAKE(src, dst)
#define CSL_EDMA3_CIDX_MAKE(src, dst)

Define Documentation

#define CSL_EDMA3_ADDRMODE_CONST   1

Address Mode is such it wraps around after reaching FIFO width

#define CSL_EDMA3_ADDRMODE_INCR   0

Address Mode is incremental

#define CSL_EDMA3_BIDX_MAKE ( src,
dst   ) 

Value:

(Uint32)(\
     CSL_FMKR(31, 16, (Uint32)dst) \
    |CSL_FMKR(15, 0 , (Uint32)src)\
    )
Used for creating the B index entry in the parameter ram

#define CSL_EDMA3_CIDX_MAKE ( src,
dst   ) 

Value:

(Uint32)(\
     CSL_FMKR(31, 16, (Uint32)dst) \
    |CSL_FMKR(15, 0,  (Uint32)src)\
    )
Used for creating the C index entry in the parameter ram

#define CSL_EDMA3_CNT_MAKE ( aCnt,
bCnt   ) 

Value:

(Uint32)(\
     CSL_FMKR(15, 0,  aCnt) \
    |CSL_FMKR(31, 16, bCnt) \
    )
Used for creating the A,B Count entry in the parameter ram

#define CSL_EDMA3_FIFOWIDTH_128BIT   4

128 bit FIFO Width

#define CSL_EDMA3_FIFOWIDTH_16BIT   1

16 bit FIFO Width

#define CSL_EDMA3_FIFOWIDTH_256BIT   5

256 bit FIFO Width

#define CSL_EDMA3_FIFOWIDTH_32BIT   2

32 bit FIFO Width

#define CSL_EDMA3_FIFOWIDTH_64BIT   3

64 bit FIFO Width

#define CSL_EDMA3_FIFOWIDTH_8BIT   0

8 bit FIFO Width

#define CSL_EDMA3_FIFOWIDTH_NONE   0

Only for ease

#define CSL_EDMA3_ITCCH_DIS   0

Intermediate transfer completion chaining disable

#define CSL_EDMA3_ITCCH_EN   1

Intermediate transfer completion chaining enable

#define CSL_EDMA3_ITCINT_DIS   0

Intermediate transfer completion interrupt disable

#define CSL_EDMA3_ITCINT_EN   1

Intermediate transfer completion interrupt enable

#define CSL_EDMA3_LINK_DEFAULT   0xFFFF

Link to a Null Param set

#define CSL_EDMA3_LINK_NULL   0xFFFF

Link to a Null Param set

#define CSL_EDMA3_LINKBCNTRLD_MAKE ( link,
bCntRld   ) 

Value:

(Uint32)(\
     CSL_FMKR(15, 0 , (Uint32)link) \
    |CSL_FMKR(31, 16, bCntRld)\
    )
Used for creating the link and B count reload entry in the parameter ram

#define CSL_EDMA3_MEMACCESS_AID0   0x0400

Allowed ID '0'

#define CSL_EDMA3_MEMACCESS_AID1   0x0800

Allowed ID '1'

#define CSL_EDMA3_MEMACCESS_AID2   0x1000

Allowed ID '2'

#define CSL_EDMA3_MEMACCESS_AID3   0x2000

Allowed ID '3'

#define CSL_EDMA3_MEMACCESS_AID4   0x4000

Allowed ID '4'

#define CSL_EDMA3_MEMACCESS_AID5   0x8000

Allowed ID '5'

#define CSL_EDMA3_MEMACCESS_EXT   0x0200

External Allowed ID. Requests with PrivID >= '6' are permitted if access type is allowed

#define CSL_EDMA3_MEMACCESS_SR   0x0020

Supervisor Read permission

#define CSL_EDMA3_MEMACCESS_SW   0x0010

Supervisor Write permission

#define CSL_EDMA3_MEMACCESS_SX   0x0008

Supervisor Execute permission

#define CSL_EDMA3_MEMACCESS_UR   0x0004

User Read permission

#define CSL_EDMA3_MEMACCESS_UW   0x0002

User Write permission

#define CSL_EDMA3_MEMACCESS_UX   0x0001

User Execute permission

#define CSL_EDMA3_OPT_MAKE ( itcchEn,
tcchEn,
itcintEn,
tcintEn,
tcc,
tccMode,
fwid,
stat,
syncDim,
dam,
sam   ) 

Value:

(Uint32)(\
     CSL_FMKR(23,23,itcchEn) \
    |CSL_FMKR(22,22,tcchEn) \
    |CSL_FMKR(21,21,itcintEn) \
    |CSL_FMKR(20,20,tcintEn) \
    |CSL_FMKR(17,12,tcc) \
    |CSL_FMKR(11,11,tccMode) \
    |CSL_FMKR(10,8,fwid) \
    |CSL_FMKR(3,3,stat) \
    |CSL_FMKR(2,2,syncDim) \
    |CSL_FMKR(1,1,dam) \
    |CSL_FMKR(0,0,sam))
Used for creating the options entry in the parameter ram

#define CSL_EDMA3_REGION_GLOBAL   -1

EDMA Regions: Global and 8 SHADOW Regions.

#define CSL_EDMA3_STATIC_DIS   0

Disable Static

#define CSL_EDMA3_STATIC_EN   1

Enable Static

#define CSL_EDMA3_SYNC_A   0

A synchronized transfer

#define CSL_EDMA3_SYNC_AB   1

AB synchronized transfer

#define CSL_EDMA3_TCC_EARLY   1

Early Completion

#define CSL_EDMA3_TCC_NORMAL   0

Normal Completion

#define CSL_EDMA3_TCCH_DIS   0

Transfer completion chaining disable

#define CSL_EDMA3_TCCH_EN   1

Transfer completion chaining enable

#define CSL_EDMA3_TCINT_DIS   0

Transfer completion interrupt disable

#define CSL_EDMA3_TCINT_EN   1

Transfer completion interrupt enable

#define CSL_EDMA3_TRIGWORD_A_B_CNT   2

Trigger word AB count

#define CSL_EDMA3_TRIGWORD_CCNT   7

Trigger word C count

#define CSL_EDMA3_TRIGWORD_DEFAULT   7

Last trigger word in a QDMA parameter set

#define CSL_EDMA3_TRIGWORD_DST   3

Trigger word destination

#define CSL_EDMA3_TRIGWORD_LINK_BCNTRLD   5

Trigger word B count reload

#define CSL_EDMA3_TRIGWORD_OPT   0

Trigger word option field

#define CSL_EDMA3_TRIGWORD_SRC   1

Trigger word source

#define CSL_EDMA3_TRIGWORD_SRC_DST_BIDX   4

Trigger word src and dst B index

#define CSL_EDMA3_TRIGWORD_SRC_DST_CIDX   6

Trigger word src and dst C index


Copyright 2011, Texas Instruments Incorporated