INTC Functions
[INTC]


Functions

CSL_Status CSL_intcGlobalEnable (CSL_IntcGlobalEnableState *prevState)
CSL_Status CSL_intcGlobalDisable (CSL_IntcGlobalEnableState *prevState)
CSL_Status CSL_intcGlobalRestore (CSL_IntcGlobalEnableState prevState)
CSL_Status CSL_intcGlobalNmiEnable (void)
CSL_Status CSL_intcGlobalExcepEnable (void)
CSL_Status CSL_intcGlobalExtExcepEnable (void)
CSL_Status CSL_intcGlobalExcepClear (CSL_IntcExcep exc)

Function Documentation

CSL_Status CSL_intcGlobalDisable ( CSL_IntcGlobalEnableState prevState  ) 

============================================================================
CSL_intcGlobalDisable

Description
Globally disable interrupts. The API disables the global interrupt by manipulating the processor's global interrupt enable/disable flag. If the user wishes to restore the enable-state at a later point, they may store the current state using the parameter, which could be used with CSL_intcGlobalRestore(..). CSL_intcGlobalDisable(..) must be called from a privileged mode.

Arguments

        prevState   (Optional) Pointer to object that would store current
                    stateObject that contains information about previous state
    

Return Value CSL_Status

Example:
        
        CSL_intcGlobalDisable(NULL);
    
=============================================================================

CSL_Status CSL_intcGlobalEnable ( CSL_IntcGlobalEnableState prevState  ) 

============================================================================
CSL_intcGlobalEnable

Description
Globally enable interrupts. The API enables the global interrupt by manipulating the processor's global interrupt enable/disable flag. If the user wishes to restore the enable-state at a later point, they may store the current state using the parameter, which could be used with CSL_intcGlobalRestore(..). CSL_intcGlobalEnable(..) must be called from a privileged mode.

Arguments

        prevState   (Optional) Pointer to object that would store current
                    stateObject that contains information about previous state
    

Return Value CSL_Status

Example:
        CSL_intcGlobalEnable(NULL);
    
=============================================================================

CSL_Status CSL_intcGlobalExcepClear ( CSL_IntcExcep  exc  ) 

============================================================================
CSL_intcGlobalExcepClear

Description
This API clears Global Exceptions

Arguments

        exc     Exception to be cleared NMI/SW/EXT/INT 
    

Return Value CSL_Status

Example:
        CSL_intcGlobalExcepClear(exc);
    
=============================================================================

CSL_Status CSL_intcGlobalExcepEnable ( void   ) 

============================================================================
CSL_intcGlobalExcepEnable

Description
This API enables global exception

Arguments

        None
    

Return Value CSL_Status

Example:
       CSL_intcGlobalExcepEnable();
    
=============================================================================

CSL_Status CSL_intcGlobalExtExcepEnable ( void   ) 

============================================================================
CSL_intcGlobalExtExcepEnable

Description
This API enables external exception

Arguments

        None
    

Return Value CSL_Status

Example:
        
        CSL_intcGlobalExtExcepEnable();
    
=============================================================================

CSL_Status CSL_intcGlobalNmiEnable ( void   ) 

============================================================================
CSL_intcGlobalNmiEnable

Description
This API enables global NMI

Arguments

        None
    

Return Value CSL_Status

Example:
        
        CSL_intcGlobalNmiEnable();
    
=============================================================================

CSL_Status CSL_intcGlobalRestore ( CSL_IntcGlobalEnableState  prevState  ) 

============================================================================
CSL_intcGlobalRestore

Description
Restore global interrupt enable/disable to a previous state. The API restores the global interrupt enable/disable state to a previous state as recorded by the global-event-enable state passed as an argument. CSL_intcGlobalRestore(..) must be called from a privileged mode.

Arguments

        prevState   Object containing information about previous state
    

Return Value CSL_Status

Example:
        CSL_IntcGlobalEnableState   prevState;
 
        CSL_intcGlobalRestore(prevState);
    
=============================================================================


Copyright 2011, Texas Instruments Incorporated