![]() |
![]() |
| CSL_TAC_BE_strmPwrMeasMode CSL_TAC_BE_getStrmPwrMeasMode | ( | ) |
CSL_TAC_BE_getStrmPwrMeasMode
Description
This function returns the accumulation mode used for the stream power measurement.
Arguments
None
Return Value
CSL_TAC_BE_strmPwrMeasMode_SlotMode The accumulation length is 1 slot (2560 chips)
CSL_TAC_BE_strmPwrMeasMode_SymbolMode The accumulation length is 1 symbol (256 chips)
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BETI_SPC_ACC_MODE
Example
CSL_TAC_BE_strmPwrMeasMode measMode;
measMode = CSL_TAC_BE_getStrmPwrMeasMode();
| void CSL_TAC_BE_getTimestamp | ( | CSL_TAC_BE_Timestamp_req * | timestamp | ) |
CSL_TAC_BE_getTimestamp
Description
This function reads the Back End Timestamp register.
Arguments
timestamp Structure with timestamp parameters.
Return Value
None
Pre Condition
None
Post Condition
None
Reads
TAC_DATA_BE_TIME_CHIP, TAC_DATA_BE_TIME_SLOT, TAC_DATA_BE_TIME_FRAME
Example
CSL_TAC_BE_Timestamp_req timestamp;
CSL_TAC_BE_getTimestamp(×tamp);
| void CSL_TAC_BE_setSwIterStart | ( | ) |
CSL_TAC_BE_setSwIterStart
Description
This function enables the Software to bypass the HW iteration start line and triggers one iteration processing on each SGCP.
This function should be used only for debugging purposes.
Arguments
None
Return Value
None
Pre Condition
None
Post Condition
The HW iteration start line is bypassed. After this point the iteration processing can be triggered only by subsequent calls to CSL_TAC_BE_setSwIterStart() API.
To take the HW out of this mode the application needs to issue a a device reset using CSL_TAC_FE_softwareReset() API.
Writes
TAC_CFG_BETI_SW_ITE_START_ITE_START=1
Example
CSL_TAC_BE_Timestamp_req timestamp;
Uint16 frame = 0;
Uint16 chip = 0;
Uint8 slot = 0;
Uint16 numIter;
// Repeat for 640 iterations
for (numIter = 0; numIter < 640; numIter++)
{
// Set the time stamp in the HW
timestamp.chipId = chip;
timestamp.slotId = slot;
timestamp.frameId = frame;
CSL_TAC_BE_setTimestamp(×tamp);
// Trigger 1 iteration worth of processing
CSL_TAC_BE_setSwIterStart();
...
// Increment the chip by 1 iteration (i.e. 4 chips)
chip += 4;
// Check for the slot boundary
if (chip == 2560)
{
// Check for the frame boundary
if (++slot == 15)
{
slot = 0;
// Check for the super frame wrap
frame = (frame + 1) & 4095;
}
}
}
| void CSL_TAC_BE_setTimestamp | ( | CSL_TAC_BE_Timestamp_req * | timestamp | ) |
CSL_TAC_BE_setTimestamp
Description
This function configures the Back End Timestamp register.
Arguments
timestamp Structure with timestamp parameters.
Return Value
None
Pre Condition
None
Post Condition
The Back-End Timestamp register is set.
Writes
TAC_DATA_BE_TIME_CHIP, TAC_DATA_BE_TIME_SLOT, TAC_DATA_BE_TIME_FRAME
Example
CSL_TAC_BE_Timestamp_req timestamp;
timestamp.chipId = 8;
timestamp.slotId = 3;
timestamp.frameId = 6;
CSL_TAC_BE_setTimestamp(×tamp);
| void CSL_TAC_BEII_clearInterrupts | ( | CSL_TAC_BEII_interruptStatus * | interruptsToClear | ) |
CSL_TAC_BEII_clearInterrupts
Description
This function clears the BEII Interrupts
Arguments
interruptsToClear Structure with the BETI interrupts to clear. A given
interrupt will be cleared if the corresponding flag
is set to 1.
Return Value
None
Pre Condition
None
Post Condition
The interrupts specified in the interruptsToClear are cleared.
Writes
TAC_CFG_BEII_ICS_SGCP0_CYC_OVER_CLR, TAC_CFG_BEII_ICS_SGCP0_FIFO_OVER_CLR, TAC_CFG_BEII_ICS_SGCP0_SEQ_CLR, TAC_CFG_BEII_ICS_SGCP0_IB_WR_MISS_CLR, TAC_CFG_BEII_ICS_SGCP1_CYC_OVER_CLR, TAC_CFG_BEII_ICS_SGCP1_FIFO_OVER_CLR, TAC_CFG_BEII_ICS_SGCP1_SEQ_CLR, TAC_CFG_BEII_ICS_SGCP1_IB_WR_MISS_CLR, TAC_CFG_BEII_ICS_BE_WD_CLR, TAC_CFG_BEII_ICS_FE_TRANS_CLR
Affects
TAC_CFG_BEII_IRS_SGCP0_CYC_OVER_STAT = 0, TAC_CFG_BEII_IRS_SGCP0_FIFO_OVER_STAT = 0, TAC_CFG_BEII_IRS_SGCP0_SEQ_STAT = 0, TAC_CFG_BEII_IRS_SGCP0_IB_WR_MISS_STAT = 0, TAC_CFG_BEII_IRS_SGCP1_CYC_OVER_STAT = 0, TAC_CFG_BEII_IRS_SGCP1_FIFO_OVER_STAT = 0, TAC_CFG_BEII_IRS_SGCP1_SEQ_STAT = 0, TAC_CFG_BEII_IRS_SGCP1_IB_WR_MISS_STAT = 0, TAC_CFG_BEII_IRS_BE_WD_STAT = 0, TAC_CFG_BEII_IRS_FE_TRANS_STAT = 0
Example
CSL_TAC_BEII_interruptStatus interruptStatus;
// Get the current interrupt status
CSL_TAC_BEII_getInterruptStatus(&interruptStatus);
// Clear all the interrupts that have occured
CSL_TAC_BEII_clearInterrupts(&interruptStatus);
| void CSL_TAC_BEII_disable | ( | ) |
CSL_TAC_BEII_disable
Description
This function disables the TAC Back End Interrupt Interface (BEII)
Arguments
None
Return Value
None
Pre Condition
None
Post Condition
The Back End Interrupt Interface is disabled.
Writes
TAC_CFG_BEII_CTRL_ENABLE=0
Example
CSL_TAC_BEII_disable();
| void CSL_TAC_BEII_disableInterrupts | ( | CSL_TAC_BEII_interruptStatus * | interruptsToDisable | ) |
CSL_TAC_BEII_disableInterrupts
Description
This function disables the BEII Interrupts
Arguments
interruptsToEnable Structure with the BETI interrupts to disable. A given
interrupt will be disabled if the corresponding flag is
set to 1.
Return Value
None
Pre Condition
None
Post Condition
The interrupts specified in the interruptsToDisable are disabled.
Writes
TAC_CFG_BEII_IECS_SGCP0_CYC_OVER_CLEAR, TAC_CFG_BEII_IECS_SGCP0_FIFO_OVER_CLEAR, TAC_CFG_BEII_IECS_SGCP0_SEQ_CLEAR, TAC_CFG_BEII_IECS_SGCP0_IB_WR_MISS_CLEAR, TAC_CFG_BEII_IECS_SGCP1_CYC_OVER_CLEAR, TAC_CFG_BEII_IECS_SGCP1_FIFO_OVER_CLEAR, TAC_CFG_BEII_IECS_SGCP1_SEQ_CLEAR, TAC_CFG_BEII_IECS_SGCP1_IB_WR_MISS_CLEAR, TAC_CFG_BEII_IECS_BE_WD_CLEAR, TAC_CFG_BEII_IECS_FE_TRANS_CLEAR
Affects
TAC_CFG_BEII_IE_SGCP0_CYC_OVER_ENA=0, TAC_CFG_BEII_IE_SGCP0_FIFO_OVER_ENA=0, TAC_CFG_BEII_IE_SGCP0_SEQ_ENA=0, TAC_CFG_BEII_IE_SGCP0_IB_WR_MISS_ENA=0, TAC_CFG_BEII_IE_SGCP1_CYC_OVER_ENA=0, TAC_CFG_BEII_IE_SGCP1_FIFO_OVER_ENA=0, TAC_CFG_BEII_IE_SGCP1_SEQ_ENA=0, TAC_CFG_BEII_IE_SGCP1_IB_WR_MISS_ENA=0, TAC_CFG_BEII_IE_BE_WD_ENA=0, TAC_CFG_BEII_IE_FE_TRANS_ENA=0
Example
CSL_TAC_BEII_interruptStatus interruptsToDisable;
// Disable the SGCP 0 FIFO Overflow interrupt
interruptsToDisable.sgcp0FifoOverStat = 1;
// Disable the BETI Watch Dog interrupt
interruptsToDisable.betiWdStat = 1;
// Don't touch the rest of the interrupts
interruptsToDisable.sgcp0CycOverStat = 0;
interruptsToDisable.sgcp0SeqStat = 0;
interruptsToDisable.sgcp0BuffMissStat = 0;
interruptsToDisable.sgcp1CycOverStat = 0;
interruptsToDisable.sgcp1FifoOverStat = 0;
interruptsToDisable.sgcp1BuffMissStat = 0;
interruptsToDisable.sgcp1SeqStat = 0;
interruptsToDisable.feTransErrStat = 0;
CSL_TAC_BEII_disableInterrupts(&interruptsToDisable);
| void CSL_TAC_BEII_enable | ( | ) |
CSL_TAC_BEII_enable
Description
This function enables the TAC Back End Interrupt Interface (BEII).
Arguments
None
Return Value
None
Pre Condition
None
Post Condition
The Back End Interrupt Interface is enabled.
Writes
TAC_CFG_BEII_CTRL_ENABLE=1
Example
CSL_TAC_BEII_enable();
| void CSL_TAC_BEII_enableInterrupts | ( | CSL_TAC_BEII_interruptStatus * | interruptsToEnable | ) |
CSL_TAC_BEII_enableInterrupts
Description
This function enables the BEII Interrupts
Arguments
interruptsToEnable Structure with the BETI interrupts to enable. A given
interrupt will be enabled if the corresponding flag is
set to 1.
Return Value
None
Pre Condition
None
Post Condition
The interrupts specified in the interruptsToEnable are enabled.
Writes
TAC_CFG_BEII_IE_SGCP0_CYC_OVER_ENA, TAC_CFG_BEII_IE_SGCP0_FIFO_OVER_ENA, TAC_CFG_BEII_IE_SGCP0_SEQ_ENA, TAC_CFG_BEII_IE_SGCP0_IB_WR_MISS_ENA, TAC_CFG_BEII_IE_SGCP1_CYC_OVER_ENA, TAC_CFG_BEII_IE_SGCP1_FIFO_OVER_ENA, TAC_CFG_BEII_IE_SGCP1_SEQ_ENA, TAC_CFG_BEII_IE_SGCP1_IB_WR_MISS_ENA, TAC_CFG_BEII_IE_BE_WD_ENA, TAC_CFG_BEII_IE_FE_TRANS_ENA
Example
CSL_TAC_BEII_interruptStatus interruptsToEnable;
// Enable the SGCP 0 FIFO Overflow interrupt
interruptsToEnable.sgcp0FifoOverStat = 1;
// Enable the BETI Watch Dog interrupt
interruptsToEnable.betiWdStat = 1;
// Don't Enable the rest of the interrupts
interruptsToEnable.sgcp0CycOverStat = 0;
interruptsToEnable.sgcp0SeqStat = 0;
interruptsToEnable.sgcp0BuffMissStat = 0;
interruptsToEnable.sgcp1CycOverStat = 0;
interruptsToEnable.sgcp1FifoOverStat = 0;
interruptsToEnable.sgcp1BuffMissStat = 0;
interruptsToEnable.sgcp1SeqStat = 0;
interruptsToEnable.feTransErrStat = 0;
CSL_TAC_BEII_enableInterrupts(&interruptsToEnable);
| void CSL_TAC_BEII_forceInterrupts | ( | CSL_TAC_BEII_interruptStatus * | interruptsToForce | ) |
CSL_TAC_BEII_forceInterrupts
Description
This function sets the BEII Interrupts
Arguments
interruptsToForce Structure with the BETI interrupts to set. A given
interrupt will be set if the corresponding flag is
set to 1.
Return Value
None
Pre Condition
None
Post Condition
The interrupts specified in the interruptsToForce are set.
Writes
TAC_CFG_BEII_IRS_SGCP0_CYC_OVER_STAT, TAC_CFG_BEII_IRS_SGCP0_FIFO_OVER_STAT, TAC_CFG_BEII_IRS_SGCP0_SEQ_STAT, TAC_CFG_BEII_IRS_SGCP0_IB_WR_MISS_STAT, TAC_CFG_BEII_IRS_SGCP1_CYC_OVER_STAT, TAC_CFG_BEII_IRS_SGCP1_FIFO_OVER_STAT, TAC_CFG_BEII_IRS_SGCP1_SEQ_STAT, TAC_CFG_BEII_IRS_SGCP1_IB_WR_MISS_STAT, TAC_CFG_BEII_IRS_BE_WD_STAT, TAC_CFG_BEII_IRS_FE_TRANS_STAT
Example
CSL_TAC_BEII_interruptStatus interruptsToForce;
// Force the SGCP 0 Cycle Overflow interrupt
interruptsToForce.sgcp0CycOverStat = 1;
// Force the SGCP 1 Input Buffer Miss Interrupt
interruptsToForce.sgcp1BuffMissStat = 1;
// Don't force the rest of the interrupts
interruptsToForce.sgcp0FifoOverStat = 0;
interruptsToForce.sgcp0SeqStat = 0;
interruptsToForce.sgcp0BuffMissStat = 0;
interruptsToForce.sgcp1CycOverStat = 0;
interruptsToForce.sgcp1FifoOverStat = 0;
interruptsToForce.sgcp1SeqStat = 0;
interruptsToForce.betiWdStat = 0;
interruptsToForce.feTransErrStat = 0;
CSL_TAC_BEII_forceInterrupts(&interruptsToForce);
| void CSL_TAC_BEII_getEnabledInterruptStatus | ( | CSL_TAC_BEII_interruptStatus * | interruptEnStatus | ) |
CSL_TAC_BEII_getEnabledInterruptStatus
Description
This function reads the BEII Interrupt Enable Status
Arguments
interruptEnStatus Structure with the BETI interrupt Enable status.
Return Value
None
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BEII_IES_SGCP0_CYC_OVER_STAT, TAC_CFG_BEII_IES_SGCP0_FIFO_OVER_STAT, TAC_CFG_BEII_IES_SGCP0_SEQ_STAT, TAC_CFG_BEII_IES_SGCP0_IB_WR_MISS_STAT, TAC_CFG_BEII_IES_SGCP1_CYC_OVER_STAT, TAC_CFG_BEII_IES_SGCP1_FIFO_OVER_STAT, TAC_CFG_BEII_IES_SGCP1_SEQ_STAT, TAC_CFG_BEII_IES_SGCP1_IB_WR_MISS_STAT, TAC_CFG_BEII_IES_BE_WD_STAT, TAC_CFG_BEII_IES_FE_TRANS_STAT
Example
CSL_TAC_BEII_interruptStatus interruptEnStatus;
CSL_TAC_BEII_getEnabledInterruptStatus(&interruptEnStatus);
if (interruptEnStatus.sgcp0CycOverStat)
{
// SGCP 0 Cycle Overflow Interrupt is enabled
...
}
| CSL_TAC_BEII_enableStatus CSL_TAC_BEII_getEnableStatus | ( | ) |
CSL_TAC_BEII_getEnableStatus
Description
This function returns the enable status of the BEII.
Arguments
None
Return Value
CSL_TAC_BEII_Disabled The BEII is disabled.
CSL_TAC_BEII_Enabled The BEII is enabled.
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BEII_CTRL_ENABLE
Example
CSL_TAC_BEII_enable();
if (CSL_TAC_BEII_getEnableStatus() != CSL_TAC_BEII_Enabled)
{
// The BEII should have been enabled.
...
}
...
CSL_TAC_BEII_disable();
if (CSL_TAC_BEII_getEnableStatus() != CSL_TAC_BEII_Disabled)
{
// The BEII should have been disabled.
...
}
| Uint32 CSL_TAC_BEII_getEOI | ( | ) |
CSL_TAC_BEII_getEOI
Description
This function returns the contents of BEII End of Interrupt register.
Arguments
None
Return Value
Uint32
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BEII_EOI_EOI
Example
Uint32 eoiVal;
eoiVal = CSL_TAC_BEII_getEOI();
| void CSL_TAC_BEII_getInterruptStatus | ( | CSL_TAC_BEII_interruptStatus * | interruptStatus | ) |
CSL_TAC_BEII_getInterruptStatus
Description
This function reads the BEII Interrupt Status
Arguments
interruptStatus Structure with the active BETI interrupt status.
Return Value
None
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BEII_IRS_SGCP0_CYC_OVER_STAT, TAC_CFG_BEII_IRS_SGCP0_FIFO_OVER_STAT, TAC_CFG_BEII_IRS_SGCP0_SEQ_STAT, TAC_CFG_BEII_IRS_SGCP0_IB_WR_MISS_STAT, TAC_CFG_BEII_IRS_SGCP1_CYC_OVER_STAT, TAC_CFG_BEII_IRS_SGCP1_FIFO_OVER_STAT, TAC_CFG_BEII_IRS_SGCP1_SEQ_STAT, TAC_CFG_BEII_IRS_SGCP1_IB_WR_MISS_STAT, TAC_CFG_BEII_IRS_BE_WD_STAT, TAC_CFG_BEII_IRS_FE_TRANS_STAT
Example
CSL_TAC_BEII_interruptStatus interruptStatus;
CSL_TAC_BEII_getInterruptStatus(&interruptStatus);
if (interruptStatus.sgcp0CycOverStat)
{
// SGCP 0 Cycle Overflow Interrupt occured
...
}
if (interruptStatus.sgcp0FifoOverStat)
{
// SGCP 0 FIFO Overflow Interrupt occured
...
}
if (interruptStatus.sgcp0SeqStat)
{
// SGCP 0 Cycle Sequencer Idle Interrupt occured
...
}
if (interruptStatus.sgcp0BuffMissStat)
{
// SGCP 0 Input Buffer Miss Interrupt occured
...
}
if (interruptStatus.sgcp1CycOverStat)
{
// SGCP 1 Cycle Overflow Interrupt occured
...
}
if (interruptStatus.sgcp1FifoOverStat)
{
// SGCP 1 FIFO Overflow Interrupt occured
...
}
if (interruptStatus.sgcp1SeqStat)
{
// SGCP 01Cycle Sequencer Idle Interrupt occured
...
}
if (interruptStatus.sgcp1BuffMissStat)
{
// SGCP 1 Input Buffer Miss Interrupt occured
...
}
if (interruptStatus.betiWdStat)
{
// The Back-End Watch Dog Timer counter reached 0
...
}
if (interruptStatus.feTransErrStat)
{
// Front-End Transaction ID unavailable
...
}
| void CSL_TAC_BEII_setEOI | ( | Uint32 | eoiVecValue | ) |
CSL_TAC_BEII_setEOI
Description
This function configures the BEII End of Interrupt register.
Arguments
eoiVecValue EOI Vector value
None
Return Value
None
Pre Condition
None
Post Condition
None
Writes
TAC_CFG_BEII_EOI_EOI
Example
CSL_TAC_BEII_setEOI(5000);
| void CSL_TAC_BETI_clearWatchDogInterrupt | ( | ) |
CSL_TAC_BETI_clearWatchDogInterrupt
Description
This function clears the interrupt registered in the watch dog interrupt status register.
Arguments
None
Return Value
None
Pre Condition
None
Post Condition
None
Writes
TAC_CFG_BETI_WINT_INT_STAT=0
Example
CSL_TAC_BETI_wdInterruptStatus wdIntStatus;
wdIntStatus = CSL_TAC_BETI_getWatchDogInterruptStatus();
if (wdIntStatus == CSL_TAC_BETI_wdInterruptStatus_Int)
{
// Interrupt generated and forwarded to BEII
CSL_TAC_BETI_clearWatchDogInterrupt();
}
| void CSL_TAC_BETI_disable | ( | ) |
CSL_TAC_BETI_disable
Description
This function disables the TAC Back End Transfer Interface (BETI).
Arguments
None
Return Value
None
Pre Condition
None
Post Condition
The Back End Transfer Interface is disabled.
Writes
TAC_CFG_BETI_CTRL_ENABLE=0
Example
CSL_TAC_BETI_disable();
| void CSL_TAC_BETI_enable | ( | ) |
CSL_TAC_BETI_enable
Description
This function enables the TAC Back End Transfer Interface (BETI).
Arguments
None
Return Value
None
Pre Condition
None
Post Condition
The Back End Transfer Interface is enabled.
Writes
TAC_CFG_BETI_CTRL_ENABLE=1
Example
CSL_TAC_BETI_enable();
| CSL_TAC_BETI_enableStatus CSL_TAC_BETI_getEnableStatus | ( | ) |
CSL_TAC_BETI_getEnableStatus
Description
This function returns the enable status of the BETI.
Arguments
None
Return Value
CSL_TAC_BETI_Disabled The BETI is disabled.
CSL_TAC_BETI_Enabled The BETI is enabled.
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BETI_CTRL_ENABLE
Example
CSL_TAC_BETI_enable();
if (CSL_TAC_BETI_getEnableStatus() != CSL_TAC_BETI_Enabled)
{
// The BETI should have been enabled.
...
}
...
CSL_TAC_BETI_disable();
if (CSL_TAC_BETI_getEnableStatus() != CSL_TAC_BETI_Disabled)
{
// The BETI should have been disabled.
...
}
| void CSL_TAC_BETI_getStatus | ( | CSL_TAC_BETI_status * | betiStatus | ) |
CSL_TAC_BETI_getStatus
Description
This function returns the BETI status indicating whether the SGCPs are Busy or Idle.
Arguments
betiStatus Status of the SGCPs
Return Value None
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BETI_STAT_SGCP0_STATUS, TAC_CFG_BETI_STAT_SGCP1_STATUS
Example
CSL_TAC_BETI_status betiStatus;
CSL_TAC_BETI_getStatus(&betiStatus);
if (betiStatus.sgcp0Status == CSL_TAC_BETI_statusBit_Idle)
{
// SGCP 0 Idle
...
}
if (betiStatus.sgcp1Status == CSL_TAC_BETI_statusBit_Busy)
{
// SGCP 1 Busy
...
}
| CSL_TAC_BETI_wdInterruptStatus CSL_TAC_BETI_getWatchDogInterruptStatus | ( | ) |
CSL_TAC_BETI_getWatchDogInterruptStatus
Description
This function reads the content of the watch dog interrupt status register.
Arguments
None
Return Value
CSL_TAC_BETI_wdInterruptStatus_NoInt No interrupt has been generated.
CSL_TAC_BETI_wdInterruptStatus_Int An interrupt has been generated and forwarded to the BEII.
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BETI_WINT_INT_STAT
Example
CSL_TAC_BETI_wdInterruptStatus wdIntStatus;
wdIntStatus = CSL_TAC_BETI_getWatchDogInterruptStatus();
if (wdIntStatus == CSL_TAC_BETI_wdInterruptStatus_Int)
{
// Interrupt generated and forwarded to BEII
...
}
| Uint16 CSL_TAC_BETI_getWatchDogStatus | ( | ) |
CSL_TAC_BETI_getWatchDogStatus
Description
This function reads the content of the BETI watch dog decounter.
Arguments
None
Return Value
Current value of the decounter.
Pre Condition
None
Post Condition
None
Reads
TAC_CFG_BETI_WST_BE_WD_STAT
Example
Uint16 deCnt;
deCnt = CSL_TAC_BETI_getWatchDogStatus();
...
| void CSL_TAC_BETI_setWatchDog | ( | Uint16 | reloadCnt | ) |
CSL_TAC_BETI_setWatchDog
Description
This function configures the watch dog in the BETI.
Arguments
reloadCnt The value indicates the number of elapsed TAC clock cycles
between DMA write accesses that will trigger a watchdog
interrupt.
Return Value None
Pre Condition
None
Post Condition
The Back-End watch-dog is configured.
Writes
TAC_CFG_BETI_WCFG_BE_WD_CFG
Example
CSL_TAC_BETI_setWatchDog(100);