TIMER Data Structures
[TIMER]


Data Structures

struct  CSL_TmrHwSetup
 Hardware setup structure. More...
struct  CSL_TmrConfig
 Config-structure Used to configure the GP timer using CSL_tmrHwSetupRaw(). More...
struct  CSL_TmrContext
 Module specific context information. Present implementation of GP timer CSL doesn't have any context information. More...
struct  CSL_TmrParam
 Module specific parameters. Present implementation of GP timer CSL doesn't have any module specific parameters. More...
struct  CSL_TmrBaseAddress
 This structure contains the base-address information for the peripheral instance. More...
struct  CSL_TmrObj
 Watchdog timer object structure. More...

Typedefs

typedef CSL_TmrObjCSL_TmrHandle
 This data type is used to return the handle to the CSL of the GP timer.

Copyright 2011, Texas Instruments Incorporated