TSC Functions
[TSC]


Functions

void CSL_tscEnable (void)
CSL_Uint64 CSL_tscRead (void)

Function Documentation

void CSL_tscEnable ( void   ) 

===========================================================================
CSL_tscEnable

Description
This API enables the 64 bit time stamp counter. The Time Stamp Counter (TSC) stops only upon Reset or powerdown. When time stamp counter is enabled (following a reset or powerdown of the CPU) it will initialize to 0 and begin incrementing once per CPU cycle. You cannot reset the time stamp counter.

Arguments
None

Return Value
None

Pre Condition
None

Post Condition
Time Stamp Counter value starts incrementing

Writes
TSCL=0, TSCH=0

Example

        
        CSL_tscEnable ();
        
 *   
============================================================================

CSL_Uint64 CSL_tscRead ( void   ) 

============================================================================
CSL_tscRead

Description
Reads the 64 bit timer stamp conter and return the 64-bit counter value.

Arguments None

Return Value CSL_Uint64

Pre Condition
None

Post Condition
None

Reads TSCL, TSCH

Example

        CSL_Uint64        counterVal;
        
        ...
        
        CSL_tscStart();
        
        ...
        
        counterVal = CSL_tscRead();
        
 *   
============================================================================


Copyright 2011, Texas Instruments Incorporated