_CSL_RAC_FE_Timestamp_req Struct Reference
[RAC Front-End Data Structures]

CSL_RAC_FE_Timestamp_req This descriptor specifies the parameters required to setup a timestamp. More...

#include <csl_rac_regsFETypes.h>


Data Fields

Uint16 chipId
Uint16 frameId
Uint8 slotId


Detailed Description

CSL_RAC_FE_Timestamp_req This descriptor specifies the parameters required to setup a timestamp.


Field Documentation

Uint16 _CSL_RAC_FE_Timestamp_req::chipId

Specifies the chip value.

Uint16 _CSL_RAC_FE_Timestamp_req::frameId

Specifies the slot value.

Uint8 _CSL_RAC_FE_Timestamp_req::slotId

Specifies the frame value.


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated