_CSL_RAC_GCCP_cycleOverflowStatus Struct Reference
[RAC GCCP Data Structures]

CSL_RAC_GCCP_cycleOverflowStatus This descriptor specifies the parameters required obtained when reading the cycle overflow status register. More...

#include <csl_rac_regsGCCPTypes.h>


Data Fields

Uint16 iteNb
Uint8 cycOverFlag
Uint8 pageIdx
Uint8 taskIdx


Detailed Description

CSL_RAC_GCCP_cycleOverflowStatus This descriptor specifies the parameters required obtained when reading the cycle overflow status register.


Field Documentation

Uint16 _CSL_RAC_GCCP_cycleOverflowStatus::iteNb

Denotes the iteration Number.

Uint8 _CSL_RAC_GCCP_cycleOverflowStatus::cycOverFlag

Denotes the cycle overflow flag.

Uint8 _CSL_RAC_GCCP_cycleOverflowStatus::pageIdx

Denotes the page index.

Uint8 _CSL_RAC_GCCP_cycleOverflowStatus::taskIdx

Denotes the task index.


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated