CSL_Aif2AtCountObj Struct Reference
[AIF2 Data Structures]

#include <csl_aif2.h>


Data Fields

Uint32 ClockNum
Uint8 SymbolNum
Uint8 LutIndexNum
Uint32 FrameLsbNum
Uint32 FrameMsbNum
Bool FcbMinusOne


Detailed Description

This object is used to query Phy/Rad timer count and timer init objects


Field Documentation

Uint32 CSL_Aif2AtCountObj::ClockNum

AT event count clock num

Uint8 CSL_Aif2AtCountObj::SymbolNum

AT event count symbol num

Uint8 CSL_Aif2AtCountObj::LutIndexNum

AT event count lut index num

Uint32 CSL_Aif2AtCountObj::FrameLsbNum

AT event count frame lsb num

Uint32 CSL_Aif2AtCountObj::FrameMsbNum

AT event count frame msb num

Bool CSL_Aif2AtCountObj::FcbMinusOne

FCB - 1 flag for Ul rad or Dl rad timer


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated