CSL_Aif2AtGsmTCount Struct Reference
[AIF2 Data Structures]

This object contains the aif2 GSM Tcount information. More...

#include <csl_aif2.h>


Data Fields

Uint16 t1
Uint8 t2
Uint8 t3


Detailed Description

This object contains the aif2 GSM Tcount information.


Field Documentation

Uint16 CSL_Aif2AtGsmTCount::t1

GSM T1 count

Uint8 CSL_Aif2AtGsmTCount::t2

GSM T2 count

Uint8 CSL_Aif2AtGsmTCount::t3

GSM T3 count


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated