CSL_Aif2AtLinkSetup Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2LinkSetup. This structure is used for configuring the parameters of aif2 timer module. More...

#include <csl_aif2.h>


Data Fields

Uint32 PiMax
Uint32 PiMin
Uint32 DeltaOffset
Bool IsNegativeDelta
Uint32 PE1Offset
Uint32 PE2Offset


Detailed Description

This is a sub-structure in CSL_Aif2LinkSetup. This structure is used for configuring the parameters of aif2 timer module.


Field Documentation

Uint32 CSL_Aif2AtLinkSetup::PiMax

Maximum pi offset value. max and min pi makes a window for pi offset

Uint32 CSL_Aif2AtLinkSetup::PiMin

Minimum pi offset value. max and min pi makes a window for pi offset

Uint32 CSL_Aif2AtLinkSetup::DeltaOffset

Delta event offset index it is calculated based on byte clock

Bool CSL_Aif2AtLinkSetup::IsNegativeDelta

Control for positive or negative delta for TM delta event. Controls the BFN PHYT frame number passed to the TM when the Delta event occurs

Uint32 CSL_Aif2AtLinkSetup::PE1Offset

PE1 event offset index it is calculated based on byte clock

Uint32 CSL_Aif2AtLinkSetup::PE2Offset

PE2 event offset index it is calculated based on byte clock


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated