CSL_Aif2AtTcObj Struct Reference
[AIF2 Data Structures]

#include <csl_aif2.h>


Data Fields

CSL_Aif2AtCountObjpPhyTimerTc
CSL_Aif2AtCountObjpRadTimerTc
Uint32 RadClockCountTc [128]


Detailed Description

This object is used to setup terminal count value for Phy and Rad timers


Field Documentation

CSL_Aif2AtCountObj* CSL_Aif2AtTcObj::pPhyTimerTc

AT event phy timer terminal count pointer

CSL_Aif2AtCountObj* CSL_Aif2AtTcObj::pRadTimerTc

AT event rad timer terminal count pointer

Uint32 CSL_Aif2AtTcObj::RadClockCountTc[128]

Rad timer Ram structure for symbol and Lut index


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated