CSL_Aif2AtWcdmaCount Struct Reference
[AIF2 Data Structures]

This object contains the aif2 wcdma count value information. More...

#include <csl_aif2.h>


Data Fields

Uint16 chip
Uint8 slot
Uint16 frame


Detailed Description

This object contains the aif2 wcdma count value information.


Field Documentation

Uint16 CSL_Aif2AtWcdmaCount::chip

WCDMA chip value

Uint8 CSL_Aif2AtWcdmaCount::slot

WCDMA slot value

Uint16 CSL_Aif2AtWcdmaCount::frame

WCDMA frame vlaue


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated