CSL_Aif2BaseAddress Struct Reference
[AIF2 Data Structures]

This will have the base-address information for the peripheral instance. More...

#include <csl_aif2.h>


Data Fields

CSL_Aif2RegsOvly regs


Detailed Description

This will have the base-address information for the peripheral instance.


Field Documentation

CSL_Aif2RegsOvly CSL_Aif2BaseAddress::regs

This is a pointer to the registers of the AIF2


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated