CSL_Aif2CpriCwLut Struct Reference
[AIF2 Data Structures]

This structure is used for dynamic configuring the cpri 256 control word LUT parameters of protocol decoder. More...

#include <csl_aif2.h>


Data Fields

Uint8 ChannelNum
Uint8 CpriCwChannel
Bool bEnableCpriCw


Detailed Description

This structure is used for dynamic configuring the cpri 256 control word LUT parameters of protocol decoder.


Field Documentation

Uint8 CSL_Aif2CpriCwLut::ChannelNum

dedicated channel number for this setup

Uint8 CSL_Aif2CpriCwLut::CpriCwChannel

All possible CPRI CW per hyperframe are are mapped to one of four(0~3) CPRI CW staging areas

Bool CSL_Aif2CpriCwLut::bEnableCpriCw

All possible CPRI CW per hyperframe. Dicatates whether the control word should be captured at all


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated