CSL_Aif2EeAif2Int Struct Reference
[AIF2 Data Structures]

This object contains the aif2 EE Aif2 Error Interrupt data information. More...

#include <csl_aif2.h>


Data Fields

Bool Error_intr
Bool Alarm_intr
Bool Cdma_intr


Detailed Description

This object contains the aif2 EE Aif2 Error Interrupt data information.


Field Documentation

Bool CSL_Aif2EeAif2Int::Error_intr

ee error interrupt

Bool CSL_Aif2EeAif2Int::Alarm_intr

ee alarm interrupt

Bool CSL_Aif2EeAif2Int::Cdma_intr

ee cppi dma interrupt


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated