CSL_Aif2EeSdInt Struct Reference
[AIF2 Data Structures]

This object contains the aif2 EE SD Interrupt data information. More...

#include <csl_aif2.h>


Data Fields

Bool sd_ee_stspll_b4_err
Bool sd_ee_stspll_b8_err


Detailed Description

This object contains the aif2 EE SD Interrupt data information.


Field Documentation

Bool CSL_Aif2EeSdInt::sd_ee_stspll_b4_err

ee serdes interrupt sd_ee_stspll_b4_err

Bool CSL_Aif2EeSdInt::sd_ee_stspll_b8_err

ee serdes interrupt sd_ee_stspll_b8_err


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated