CSL_Aif2FrameCounter Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2Pd(Pe)CommonSetup. This structure is used for configuring the parameters of PD, PE frame counter. More...

#include <csl_aif2.h>


Data Fields

Uint8 FrameIndexTc
Uint8 FrameIndexSc
Uint8 FrameSymbolTc


Detailed Description

This is a sub-structure in CSL_Aif2Pd(Pe)CommonSetup. This structure is used for configuring the parameters of PD, PE frame counter.


Field Documentation

Uint8 CSL_Aif2FrameCounter::FrameIndexTc

OBSAI AxC framing counter. Index Terminal count.

Uint8 CSL_Aif2FrameCounter::FrameIndexSc

OBSAI AxC framing counter. Index Start count.

Uint8 CSL_Aif2FrameCounter::FrameSymbolTc

OBSAI AxC framing counter. Symbol terminal count


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated