CSL_Aif2GlobalSetup Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2HwSetup. This structure is used for configuring the parameters global to AIF2. More...

#include <csl_aif2.h>


Data Fields

Bool ActiveLink [6]
CSL_Aif2FrameMode frameMode


Detailed Description

This is a sub-structure in CSL_Aif2HwSetup. This structure is used for configuring the parameters global to AIF2.


Field Documentation

Bool CSL_Aif2GlobalSetup::ActiveLink[6]

Active link flag

CSL_Aif2FrameMode CSL_Aif2GlobalSetup::frameMode

frame mode : Normal mode , Short frame mode


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated