CSL_Aif2LinkSetup Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2HwSetup. This structure is used for configuring the parameters of an outbound link. More...

#include <csl_aif2.h>


Data Fields

CSL_Aif2LinkIndex linkIndex
CSL_Aif2SdLinkSetuppSdLinkSetup
CSL_Aif2CommonLinkSetuppComLinkSetup
CSL_Aif2TmLinkSetuppTmLinkSetup
CSL_Aif2RtLinkSetuppRtLinkSetup
CSL_Aif2PeLinkSetuppPeLinkSetup
CSL_Aif2PdLinkSetuppPdLinkSetup
CSL_Aif2AtLinkSetuppAtLinkSetup


Detailed Description

This is a sub-structure in CSL_Aif2HwSetup. This structure is used for configuring the parameters of an outbound link.


Field Documentation

CSL_Aif2LinkIndex CSL_Aif2LinkSetup::linkIndex

Link index 0-5

CSL_Aif2SdLinkSetup* CSL_Aif2LinkSetup::pSdLinkSetup

pointer to Sd link setup

CSL_Aif2CommonLinkSetup* CSL_Aif2LinkSetup::pComLinkSetup

pointer to link common setup

CSL_Aif2TmLinkSetup* CSL_Aif2LinkSetup::pTmLinkSetup

pointer to TM setup

CSL_Aif2RtLinkSetup* CSL_Aif2LinkSetup::pRtLinkSetup

pointer to re-transmitter link setup

CSL_Aif2PeLinkSetup* CSL_Aif2LinkSetup::pPeLinkSetup

pointer to protocol encoder link setup

CSL_Aif2PdLinkSetup* CSL_Aif2LinkSetup::pPdLinkSetup

pointer to Protocol decoder link setup

CSL_Aif2AtLinkSetup* CSL_Aif2LinkSetup::pAtLinkSetup

pointer to Aif2 timer link setup (Pi, Delta, PE signal)


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated